This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354:矩阵键盘的GPIO驱动修改



你好,我使用

SDK: PROCESSOR-SDK-LINUX-AM335X  06_03_00_106

根文件系统: tisdk-image-am335x-evm

对设备树进行了以下修改:

matrix_keypad: matrix_keypad@0 {
                compatible = "gpio-matrix-keypad";
                debounce-delay-ms = <5>;
                col-scan-delay-us = <2>;

                row-gpios = <&gpio1 16 GPIO_ACTIVE_HIGH         /* Bank1, pin25 */
                             &gpio1 19 GPIO_ACTIVE_HIGH         /* Bank1, pin26 */
                             &gpio1 23 GPIO_ACTIVE_HIGH
                             &gpio1 24 GPIO_ACTIVE_HIGH         /* Bank1, pin26 */
                             &gpio1 25 GPIO_ACTIVE_HIGH
			     &gpio1 26 GPIO_ACTIVE_HIGH         /* Bank1, pin25 */
                             &gpio1 27 GPIO_ACTIVE_HIGH         /* Bank1, pin26 */
                             &gpio1 13 GPIO_ACTIVE_HIGH>;       /* Bank1, pin27 */

                col-gpios = <&gpio1 18 GPIO_ACTIVE_HIGH         /* Bank1, pin21 */
			     &gpio1 21 GPIO_ACTIVE_HIGH         /* Bank1, pin21 */
                             &gpio1 22 GPIO_ACTIVE_HIGH>;       /* Bank1, pin22 */


                linux,keymap = <0x0001003b      /* MENU */
                                0x0002003c      /* BACK */
                                0x0100003d      /* LEFT */
                                0x0102003e      /* RIGHT */
                                0x0200003f      /* ENTER */
                                0x02000040      /* BACK */
                                0x03000041      /* LEFT */
                                0x03010042      /* RIGHT */
                                0x03020043      /* ENTER */
				0x04000044
                                0x04010045      /* RIGHT */
                                0x04020046      /* ENTER */
                                0x05000047      /* BACK */
                                0x05010048      /* LEFT */
                                0x06000049      /* RIGHT */
                                0x0601004a      /* ENTER */
                                0x0602004b
                                0x0700004c      /* RIGHT */
                                0x0701004d      /* ENTER */
                                0x0702004e>;    /* DOWN */
        };
matrix_keypad_s0: matrix_keypad_s0 {
pinctrl-single,pins = <
AM33XX_IOPAD(0x840, PIN_INPUT_PULLUP | MUX_MODE7) /* gpmc_a0.gpio1 16 */
AM33XX_IOPAD(0x84c, PIN_INPUT_PULLUP | MUX_MODE7) /* gpmc_a3.gpio1 19 */
AM33XX_IOPAD(0x85c, PIN_INPUT_PULLUP | MUX_MODE7) /* gpmc_a7.gpio1 23 */
AM33XX_IOPAD(0x860, PIN_INPUT_PULLUP | MUX_MODE7) /* gpmc_a8.gpio1 24 */
AM33XX_IOPAD(0x864, PIN_INPUT_PULLUP | MUX_MODE7) /* gpmc_a9.gpio1 25 */
AM33XX_IOPAD(0x868, PIN_INPUT_PULLUP | MUX_MODE7) /* gpmc_a10.gpio1 26 */
AM33XX_IOPAD(0x86c, PIN_INPUT_PULLUP | MUX_MODE7) /* gpmc_a11.gpio1 27 */
AM33XX_IOPAD(0x834, PIN_INPUT_PULLUP | MUX_MODE7) /* gpmc_ad13.gpio1 13 */

AM33XX_IOPAD(0x848, PIN_OUTPUT_PULLUP | MUX_MODE7) /* gpmc_a2.gpio1 18 */
AM33XX_IOPAD(0x854, PIN_OUTPUT_PULLUP | MUX_MODE7) /* gpmc_a5.gpio1 21 */
AM33XX_IOPAD(0x858, PIN_OUTPUT_PULLUP | MUX_MODE7) /* gpmc_a6.gpio1 22 */

>;
};


上电按键无反应
root@am335x-evm:/dev/input/by-path# evtest /dev/input/event1

Input driver version is 1.0.1

Input device ID: bus 0x19 vendor 0x0 product 0x0 version 0x0

Input device name: "matrix_keypad@0"

Supported events:
  
Event type 0 (EV_SYN)
  
Event type 1 (EV_KEY)
    
Event code 59 (KEY_F1)
    
Event code 60 (KEY_F2)
    
Event code 61 (KEY_F3)
    
Event code 62 (KEY_F4)
    
Event code 63 (KEY_F5)
    
Event code 64 (KEY_F6)
    
Event code 65 (KEY_F7)
    
Event code 66 (KEY_F8)
    
Event code 67 (KEY_F9)
    
Event code 68 (KEY_F10)
    
Event code 69 (KEY_NUMLOCK)
    
Event code 70 (KEY_SCROLLLOCK)
    
Event code 71 (KEY_KP7)
    
Event code 72 (KEY_KP8)
    
Event code 73 (KEY_KP9)
    
Event code 74 (KEY_KPMINUS)
    
Event code 75 (KEY_KP4)
    
Event code 76 (KEY_KP5)
    
Event code 77 (KEY_KP6)
    
Event code 78 (KEY_KPPLUS)
  
Event type 4 (EV_MSC)
    
Event code 4 (MSC_SCAN)

Key repeat handling:
  
Repeat type 20 (EV_REP)
    
Repeat code 0 (REP_DELAY)
      Value    250
    
Repeat code 1 (REP_PERIOD)
      Value     33

Properties:Testing ... (interrupt to exit)

测试发现 gpmc_a2.、 gpmc_a5.、pmc_a6.三脚均输出高电平,按键并无下拉,请问是哪里修改错误了吗?

  • 请参考am335x GPEVM的keypad部分原理图以及am335x-evm.dts中的keypad配置看一下。
    processor-sdk-linux\arch\arm\boot\dts\am335x-evm.dts
    processor-sdk-linux\Documentation\devicetree\bindings\input\gpio-matrix-keypad.txt
  • 目前的dts便是参考以上两个文件编写的。

    am335xevm中的矩阵键盘好像与CPLD相连,我的电路如下:

  • ZB_LAJI 说:

    测试发现 gpmc_a2.、 gpmc_a5.、pmc_a6.三脚均输出高电平,按键并无下拉,请问是哪里修改错误了吗?

    能将原理图截图看一下吗?

    将gpmc_a2/ gpmc_a5/gpmc_a6根据实际情况修改成高有效或者低有效可以吗?

     col-gpios = <&gpio1 18 GPIO_ACTIVE_HIGH         /* Bank1, pin21 */
    			     &gpio1 21 GPIO_ACTIVE_HIGH         /* Bank1, pin21 */
                                 &gpio1 22 GPIO_ACTIVE_HIGH>;       /* Bank1, pin22 */

    或者测试一个简单的gpio key测试看看。

  • 原理图就是上一个帖子的图片,
    电路图原理为一开始输出均为低电平,当按键按下,输入检测到低,表面某一列按键中有一个按下,所以所有输出先均拉高,再逐一输出低电平,以此判断哪一个按键按下。
    已尝试过修改成高有效或者低,无变化。