This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 网口无法与PC通信



现象描述:

使用第三方的硬件板,设计与EVM一致(DDR时钟与SRIO时钟),但在网口上使用的是SGMII1,而EVM板使用的是SGMII0。我曾经在硬件板上测试网口是可以通信的,但是放置一段时间后,由于没有留存先前代码,重新建立工程测试,发现已经无法和PC通信了。

我的代码来源以及调试过程如下:

首先,我修改了PDK目录(pdk_C6678_1_1_2_6\packages\ti\platform\evmc6678l\)下的6678平台库中的platform.c文件,将Init_SGMII(1)修改为Init_SGMII(0),因为时钟和EVM板一致,故没有做其他的修改,rebuild此库。然后,我在MCSDK提供的Helloworld程序中,修改了IP地址,让PC和DSP处于同一网段内,以及禁用了DHCP,rebuild工程,下载。打印输出如下信息:

--------------------------------------------------------------------

[C66xx_0] QMSS successfully initialized  
CPPI successfully initialized  
PA successfully initialized  
 
TCP/IP Stack 'Hello World!' Application 
 
TCP/IP Stack 'Hello World!' Application 
 
PASS successfully initialized  
Ethernet subsystem successfully initialized  
Ethernet eventId : 48 and vectId (Interrupt) : 7  
Registration of the EMAC Successful, waiting for link up .. 
Network Added: If-1:169.254.98.1
------------------------------------------------------------------

但是使用PC ping却无法ping通 ,结果如下:

我排查了网线的问题(连接两台PC是可以ping通的)

此外,我使用了STK中的GE程序,进行回环测试,都是通过的。然后进行如下代码修改,切换到DSP0到DSP1的测试模式,

/*select between internal/external loopback test or test between two DSPs*/
//GE_Test_Data_Path test_data_path= GE_TEST_SERDES_LOOPBACK;//modify
GE_Test_Data_Path test_data_path= GE_TEST_DSP0_TO_DSP1;

/*select between 10/100/1000Mbps or auto negotiation mode*/
//Ethernet_Mode ethernet_mode = ETHERNET_1000M_FULLDUPLEX;//modify
Ethernet_Mode ethernet_mode = ETHERNET_AUTO_NEGOTIAT_SLAVE;
//The port connection state for the test
GE_Port_Connection port_connect[GE_NUM_ETHERNET_PORT]=
{
//	GE_PORT_NO_CONNECT, //SGMII port 0 //modify
      GE_PORT_CABLE_CONNECT, //SGMII port 0
     GE_PORT_NOT_USED//SGMII 1 };

并且将目标MAC也修改为PC的MAC。

rebuild,load之后。则打印信息显示wait for port 0 phy link ,如图:

发现是在如下代码中一直循环:

while(0==(gpMDIO_regs->LINK_REG&(1<<i)))
{
	if(TSC_count_cycle_from(uiStartTSC)>0x3FFFFFFF)
	{
		printf("Wait for port %d PHY link...\n", i);
		uiStartTSC= TSCL;
	}
}

检查gpMDIO_regs->LINK_REG的值,为0;

但是上述程序,在EVM板上则是完全可以跑通的,可以实现与PC的通信。

在论坛上看了很多帖子,发现很多人都遇到这个问题,我理解的是:这个现象大致是DSP与PHY芯片之间没有link成功。但是是什么原因导致link不成功,不太明确,我现在遇到这个问题也是非常头疼,完全没有解决的思路~

烦请各位大佬拨冗指导一下!非常感谢

其他信息:

芯片型号:6678

MCSDK/Processor SDK版本:mcsdk_2_01_02_06  pdk_C6678_1_1_2_6

CCS版本:6.2
OS:windows 10