This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tda4 vm支持三星lpddr4吗



您好,我们想在  tda4 vm开发版上 ,适配三星的lpddr4(型号K4FBE3D4HM-TFCL),在uboot时卡住了。

错误信息如下:

U-Boot SPL 2020.01-dirty (Mar 31 2021 - 14:04:01 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0014 '20.8.5--v2020.08b (Terrific Lla')
Reading on-board EEPROM at 0x50 failed -1
j721e_ddrss_probe(dev=41c87c28)                                                                                                                                    
j721e_ddrss_ofdata_to_priv(dev=41c87c28)                                                                                                                           
j721e_ddrss_power_on(ddrss=41cda7c4)                                                                                                                               
LPDDR4_Probe: PASS                                                                                                                                                 
LPDDR4_Init: PASS                                                                                                                                                  
--->>> LPDDR4 Initialization is in progress ... <<<---                                                                                                             
counter:10                                                                                                                                                         
j721e_lpddr4_ack_freq_upd_req: received freq change req: req type = 1, req no. = 0                                                                                 
j721e_lpddr4_ack_freq_upd_req: received freq change req: req type = 0, req no. = 1                                                                                 
j721e_lpddr4_ack_freq_upd_req: received freq change req: req type = 1, req no. = 2                                                                                 
j721e_lpddr4_ack_freq_upd_req: received freq change req: req type = 0, req no. = 3                                                                                 
j721e_lpddr4_ack_freq_upd_req: received freq change req: req type = 1, req no. = 4                                                                                 
wait_for_bit_le32: Timeout (reg=114080 mask=80 wait_set=)                                                                                                          
Timeout during frequency handshake                                                                                                                               
### ERROR ### Please RESET the board ###

请问该怎么解决,非常感谢