This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About 3359 SDARM increase capacity



hi:

   你好,我这边有个3359项目,需要增加SDARM容量(2片MT47H256M8并联  从原来的256M扩容到512M)出现问题,提示加载不成功,还是256M,请问下 如何改代码 ,才可完成扩容事情 。以下是我修改后的代码可做为参考, 路径为 u-boot-2011.09-psp04.06.00.07\include\configs\Am335x_evm.h

#define CONFIG_NR_DRAM_BANKS 2 /* CS1 may or may not be populated */ #define PHYS_DRAM_1  0x8000000 /* DRAM Bank #1 */

#define PHYS_DRAM_1_SIZE 0x20000000   //512M #define PHYS_DRAM_2  0xA0000000 //512M (0x20000000+0x8000000)

#define CONFIG_SYS_SDRAM_BASE  PHYS_DRAM_1  

 #define CONFIG_SYS_INIT_RAM_ADDR SRAM0_START

 #define CONFIG_SYS_INIT_RAM_SIZE SRAM0_SIZE

#define CONFIG_SYS_INIT_SP_ADDR  (CONFIG_SYS_INIT_RAM_ADDR + \       CONFIG_SYS_INIT_RAM_SIZE - \          GENERATED_GBL_DATA_SIZE)