This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28388 的CM侧能否配置成GPIO外部中断?



手册中说可以将GPIO配置成CPU1的外部中断,那么能配置成CM侧的外部中断吗?如何实现?

Configuring external interrupts is a two-step process. First, the interrupts themselves must be enabled
and their polarity must be configured via the XINTnCR registers. Second, the XINT1-5 GPIO pins must
be set by selecting the sources for Input X-BAR signals 4, 5, 6, 13, and 14, respectively. For more
information on the Input X-BAR architecture, see the Crossbar(XBAR) chapter of this manual.