官网介绍CCS安装的网页上显示:
1 This section is applicable only if you are loading a HLOS (Linux or QNX) application.表示CCS 可以loading HLOS上的application
下面一行:
CCS cannot be used to debug applications on the A72. For Linux, it is recommended to use gdb which comes preinstalled on the filesystem. For QNX, it is recommended to use QNX Momentics.
表示CCS不能用于调试A72上的application。
到底CCS可以调试A72上(HLOS)的application么?