This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tda4 sd卡uboot failed



您好,tda4 evm custom板,16G的SamDisk sd卡,已经分区和安装好了uboot,

启动时出现如下问题:

LPDDR4_Start: PASS
Trying to boot from MMC2
Loading Environment from MMC... *** Warning - No MMC card found, using default environment

Starting ATF on ARM64 core...

NOTICE:  BL31: v2.3():07.01.00.004-1-g52c334fc3-dirty
NOTICE:  BL31: Built : 18:17:14, Nov 19 2020

U-Boot SPL 2020.01-dirty (Apr 16 2021 - 10:31:23 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0014 '20.8.5--v2020.08b (Terrific Lla')
Reading on-board EEPROM at 0x50 failed -1
Trying to boot from MMC2
i2c_write: error waiting for data ACK (status=0x116)
Error reading output register
spl: mmc init failed with error: -110
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
请问是什么问题,应该怎么解决。