This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657中MSM大小与文档不一致问题以及不同内存数据使用问题



我在6657DSP中使用MSM内存,根据文档,大小为1M,但是根据起始地址0C000000-0C1FFFFF,大小为2M,请问这是什么意思。而且我往MSM的0C000000-0C1FFFFF循环写满数字,都能正常读到,那么是不是可以在cmd中开辟为2M的空间大小?

另外,如果我只用到核0,那么对于L2、MSM、核0的L2,是不是可以进行直接的数据搬移使用?还是仍然需要借助EDMA搬运?

比如我的数组1-s[20]定义在L2中,那我定义在核0L2中的数组2-D[20],是否可以直接操作数据,比如s[i]=D[i]?

感谢回答!