您好,我在用CCS3.3来调试C6713,我想在C6713上运行一个很简单的程序,正确编译并load program后,点击run,运行一段时间之后出现“ The application is using 64 MB of DSP memory. Verify pplication memory usage. To increase the supported memory limit, refer SPRU600. ”的错误。我根据网上搜索到的结果,更改了CMD文件中的heap值,也尝试了在simulator.cfg文件中更改“MEM_USAGE_LIMIT 100”, 但这依然导致了错误产生,并且错误变为“ The application is using 100 MB of DSP memory. ”。请问这个问题是什么原因导致的?我要怎么解决呢?