在OMAPL138C6748 ROM Bootloader Resources and FAQ.pdf中,有如下介绍
2.2 Serial Boot and Flash Loading Utility
This package contains a set of utilities running from the command-line on Windows for flashing the NAND,
NOR, and serial peripheral interface (SPI) Flash of the OMAP-L138 EVM via the serial port.
The latest source code and binaries can be downloaded from TI Git.
The Serial Boot and Flash Loading Utility (which offers the same functionality as a previous program
called DVFlasher) executable is called sfh_OMAP-L138.exe.
These programs each encapsulate a distinct binary UBL that is transferred via the universal asynchronous
receiver/transmitter (UART). This implies that the chip must be operating in the UART boot mode, showing
the BOOTME prompt.
通过点击 TI Git.链接未找到文档中提到的source code and binaries