This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678给dsp 发包



dsp srio回环测试例程第29行,对于发包和收包的地址为什么总有warning (test_2DSP_cfg结构体中)

{SRIO_PKT_TYPE_SWRITE, ((Uint32)&packetBuffer_LL2_Size1[0][0])+0x10000000, ((Uint32)&packetBuffer_LL2_Size1[1][0])+0x10000000, LL2_PACKET_BUFFER_SIZE1}

Description Resource Path Location Type
#172-D pointer points outside of underlying object SRIO_2DSP_Test.c /Copy of SRIO/src line 29 C/C++ Problem