我想问下现在DVRRDK3.0里面做up-sampler是用哪个模块LINK?我看到好像Composite SwMs 可以做这个YUV420->YUV422,但是不知道输出能不能再接上SCR_LINK和NSF_LINK到YUV420送编码?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想问下现在DVRRDK3.0里面做up-sampler是用哪个模块LINK?我看到好像Composite SwMs 可以做这个YUV420->YUV422,但是不知道输出能不能再接上SCR_LINK和NSF_LINK到YUV420送编码?
SCLR link, SWMS link, DEI link都可以做UP Sample。
你说的数据通路是可行的,不过需要注意的是,编码link只可以有1个。
但是SCLR link资料里面已经说了只支持422i进出啊,SWMS link虽然可以做420sp-422i,但是link输出是给显示的,demo里面还没有下一级是送编码的, DEI link的话现在程序里面暂时是这么设置的,但是创建Link的时候会出错,现在就是想实现vdec->sclr->venc这个数据流,但是sclr只支持422,所以我想先得把420up到422才行。但是直接vdec->dei(sc)->venc的话会出错,请问专家那种方法能实现这种需求?
SC本身是422进出,这个没错。但是SCRL link不仅仅包含SC,还包含了前级的UP_SAMPLER。所以对link而言,它的输入可以是420输入的,当420输入时,数据会先经过up-sampler再进入SC。
所以两个概念,上面资料里说的是SC这个硬件单元,但SCRL link是封装过后的单元,包含up-sampler硬件和SC硬件。