This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 dvrrdk3.0 怎么使用音频输入?



平台dm8168,dvrrdk3.0开发板,我用线一端接入开发板的音频输入1口,一端接入播放歌曲的手机耳机口;摄像头接入视频输入1口,运行gui程序后,我录制的视频和现场都没有听到声音,gui里的音频设置我都设为enable了,请大家帮忙给点意见?谢谢了!

  • 你使用的是TI的EVM么?

  • 我使用的是udwork的DM8168,dvrrdk3.0的

  • GUI的不是很清楚,不过你可以在liunx的ALSA utils试一下音频,下面是一个loopback的例子:

    arecord -Dhw:0,0 -r8000 -fS16_LE -twav -c2 | aplay -Dhw:0,1 -r8000 -fS16_LE -c1

    arecord -Dhw:0,0 -r8000 -fS16_LE -twav -c2 | aplay -Dhw:0,1 -r8000 -fS16_LE -c1

  • 谢谢louis! 我按照你给的例子,我在开发板的根目录下执行,但是报错了:arecord:pcm_rea:1773:read error:Input/output error .这是怎么回事?我昨天运行mcfw 可以录制音频了,播放是有声音的,但是运行gui后录制实时的都没有声音?

  • 你用arecord -l 看一下你的设备有哪些?我给的只是一个例子,需要根据你的硬件配置,修改一下命令的参数。

  • 谢谢louis!

    root@dvr:/# aplay -l
    **** List of PLAYBACK Hardware Devices ****
    card 0: SOUND0 [TI81XX SOUND0], device 1: AIC3X tlv320aic3x-hifi-1 []
      Subdevices: 1/1
      Subdevice #0: subdevice #0
    card 1: SOUND1 [TI81XX SOUND1], device 0: hdmi HDMI-DAI-CODEC-0 []
      Subdevices: 1/1
      Subdevice #0: subdevice #0
    root@dvr:/# arecord -l
    **** List of CAPTURE Hardware Devices ****
    card 0: SOUND0 [TI81XX SOUND0], device 0: TVP-PCM tvp5158-hifi-0 []
      Subdevices: 1/1
      Subdevice #0: subdevice #0
    card 0: SOUND0 [TI81XX SOUND0], device 1: AIC3X tlv320aic3x-hifi-1 []
      Subdevices: 1/1

      Subdevice #0: subdevice #0

    这是我的具体硬件配置, 我的音频输入接到开发板的音频1口,液晶电视接入开发板的hdmi0口, 运行

    1.root@dvr:/# arecord -Dhw:0,0 -r8000 -fS16_LE -twav -c2|aplay -Dhw:0,0 -r8000 -fS
       16_LE -c1
       aplay: main:660: audio open error: No such file or directory
       Recording WAVE 'stdin' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo
       root@dvr:/# arecord -Dhw:0,0 -r8000 -fS16_LE -twav -c2|aplay -Dhw:0,1 -r8000 -fS
      16_LE -c1
      Recording WAVE 'stdin' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo
      Playing WAVE 'stdin' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo
      arecord: pcm_read:1773: read error: Input/output error

    2.root@dvr:/usr/share/sounds/alsa# aplay -Dhw:0,0 Side_Right.wav
       aplay: main:660: audio open error: No such file or directory
       root@dvr:/usr/share/sounds/alsa# aplay -Dhw:0,1 Side_Right.wav
       Playing WAVE 'Side_Right.wav' : Signed 16 bit Little Endian, Rate 48000 Hz, Mono
       aplay: set_params:1065: Channels count non available

    以上是我的音频测试信息,麻烦你帮我看看!

     

     

     

     

     

  • 运行aplay -Dhw:0,1  /input_48k.wav没报错了,但是不知道这个输出的声音接口在哪?是hdmi0口,还是开发板上的stereo audio out口?