This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385的bootargs问题

Other Parts Discussed in Thread: DM385

DM385的板子,原来是用nfs挂在文件系统的,能正常运行

bootargs=root=/dev/nfs console=ttyO0,115200n8 mem=54M rw notifyk.vpssm3_sva=0xBFD00000 nfsroot=192.168.86.253:/opt/prj/dm385/sdk/Source/ipnc_rdk/target/filesys,nolock,tcp ip=dhcp eth=00.0C.0C.02.38.45 cmemk.phys_start=0x83600000 cmemk.phys_end=0x85600000 cmemk.allowOverlap=1 earlyprintk

现在使用nand上的文件系统:

setenv bootargs console ttyO0,115200n8 rootwait=1 rw ubi.mtd=4,2048 rootfstype=ubifs root=ubi0:rootfs init=/init mem=54M vram=4M notifyk.vpssm3_sva=0xBFD00000 ip=dhcp eth=$(ethaddr) cmemk.phys_start=0x85000000 cmemk.phys_end=0x89000000 cmemk.allowOverlap=1 earlyprintk

确定nand上有文件系统,仅仅更改了bootargs,其他的一切都没有变,可怎么也启动不了。

启动信息:

Hit any key to stop autoboot:  0

Loading from nand0, offset 0x280000
   Image Name:   Linux-2.6.37_DM385_IPNC_3.50.00
   Created:      2012-12-21  11:57:15 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2483292 Bytes = 2.4 MiB
   Load Address: 80008000
   Entry Point:  80008000
## Booting kernel from Legacy Image at 81000000 ...
   Image Name:   Linux-2.6.37_DM385_IPNC_3.50.00
   Created:      2012-12-21  11:57:15 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2483292 Bytes = 2.4 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

就在这个地方停了下来,试了很多,都还是这样!

有谁知道如何解决这个问题吗?谢谢了!