This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6455: srio是否支持4个1x模式同时以3.125G的速度工作

Part Number: TMS320C6455


我使用TMS320C6455芯片的srio功能,目前port0与port1分别接了一个V7,port2与port3接到了ZYNQ7045。

经过调试发现port0与port1的链路是通的,而port2或者port3的链路不通。我们每个LineSpeed为3.125G。

我的每个port配置完全相同,查看寄存器配置也是相同。但是与ZYNQ7045的x1模式一直不通,经过测试我们排除了ZYNQ7045端的问题。

请问TMS320C6455是否支持4个1x模式同时工作,如果支持请问需要如何去配置呢?

谢谢!