This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5534: 在没有外部程序存储芯片的情况下,如何通过BootLoader中的USB方式将最终代码加载到C5534的RAM上,并在加载结束后重枚举设备。

Part Number: TMS320C5534

您好!

       我需要将我的最终代码(.bin)通过C55xx BootLoader 中的USB方式自动加载到芯片的RAM上,我看过C55xx系列的BootLoader文档,其中提到一个usb_boot.exe的工具,的确可以将我的代码烧写到芯片上,但是这个工具需要安装一个烧写驱动,烧写结束后,需要卸载这个驱动,通过C5517_WINUSB.inf文件安装一个WinUSB驱动,才能和我的上位机程序进行数据交互,这个过程需手动更换驱动,请问TI是否支持通过USB方式自动向芯片烧写程序,并自动切换驱动的方法,我没有找到这方面的资料,如果有的话,麻烦您提供相关资料的连接,万分感谢! 

     另外,我的板子上没有设额外的程序存储芯片,所以需要通过USB方式加载到目标芯片的RAM上。这个过程应该和AN2131这个USN芯片的驱动过程类似,首先通过一个驱动加载我们的代码到芯片上,然后更改驱动,转入到正常运行模式!

.