Other Parts Discussed in Thread: TFP410, TPS65217, AM3352
您好,
我用的两个phy芯片是AR8031,rgmii接口
修改设备树文件am335x-bone-common.dtsi内容如下:
cpsw_default: cpsw_default {
pinctrl-single,pins = <
/* Slave 1 */
0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txen.rgmii1_tctl */
0x118 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxdv.rgmii1_rctl */
0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd3.rgmii1_td3 */
0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd2.rgmii1_td2 */
0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.rgmii1_td1 */
0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd0.rgmii1_td0 */
0x12c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txclk.rgmii1_tclk */
0x130 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxclk.rgmii1_rclk */
0x134 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd3.rgmii1_rd3 */
0x138 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd2.rgmii1_rd2 */
0x13c (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd1.rgmii1_rd1 */
0x140 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd0.rgmii1_rd0 */
/* Slave 2 */
0x40 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a0.rgmii2_tctl */
0x44 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a1.rgmii2_rctl */
0x48 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a2.rgmii2_td3 */
0x4c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a3.rgmii2_td2 */
0x50 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a4.rgmii2_td1 */
0x54 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a5.rgmii2_td0 */
0x58 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a6.rgmii2_tclk */
0x5c (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a7.rgmii2_rclk */
0x60 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a8.rgmii2_rd3 */
0x64 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a9.rgmii2_rd2 */
0x68 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a10.rgmii2_rd1 */
0x6c (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a11.rgmii2_rd0 */
>;
};
cpsw_sleep: cpsw_sleep {
pinctrl-single,pins = <
/* Slave 1 reset value */
0x114 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x118 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x11c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x120 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x124 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x128 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x12c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x130 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x134 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x138 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x13c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x140 (PIN_INPUT_PULLDOWN | MUX_MODE7)
/* Slave 2 reset value*/
0x40 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x44 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x48 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x4c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x50 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x54 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x58 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x5c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x60 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x64 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x68 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x6c (PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <4>;
phy-mode = "rgmii";
dual_emac_res_vlan = <4>;
};
&cpsw_emac1 {
phy_id = <&davinci_mdio>, <5>;
phy-mode = "rgmii";
dual_emac_res_vlan = <5>;
};
&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
dual_emac = <1>;
status = "okay";
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
};
--------------------------------------------------------------------------------------------------------------------------------
启动log如下:
U-Boot SPL 2014.07-gfb6ab76 (Jul 06 2015 - 16:00:22)
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
U-Boot 2014.07-gfb6ab76 (Jul 06 2015 - 16:00:22)
I2C: ready
DRAM: 512 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
Net: <ethaddr> not set. Validating first E-fuse MAC
Phy not found
cpsw, usb_ether
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
** Unable to read file uEnv.txt **
4340120 bytes read in 263 ms (15.7 MiB/s)
32587 bytes read in 22 ms (1.4 MiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x423998 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8fff5000, end 8fffff4a ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 3.14.43-g875c69b (qjrobot@qjrobot-PC) (gcc version 4.9.2 20140811 (prerelease) (crosstool-NG linaro-1.13.1-4.9-2014.08 - Linaro GCC 4.9-2014.08) ) #3 Thu Jun 17 13:59:28 CST 2021
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x BeagleBone
[ 0.000000] cma: CMA: reserved 24 MiB at 9e000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129792
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 485044K/523264K available (5983K kernel code, 303K rwdata, 2148K rodata, 261K init, 232K bss, 38220K reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc07f90d4 (8133 kB)
[ 0.000000] .init : 0xc07fa000 - 0xc083b5c4 ( 262 kB)
[ 0.000000] .data : 0xc083c000 - 0xc0887d20 ( 304 kB)
[ 0.000000] .bss : 0xc0887d20 - 0xc08c1e28 ( 233 kB)
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000010] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956969942ns
[ 0.000026] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000235] Console: colour dummy device 80x30
[ 0.000254] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000259] This ensures that you still see kernel messages. Please
[ 0.000264] update your kernel commandline.
[ 0.000281] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.089545] pid_max: default: 32768 minimum: 301
[ 0.089629] Security Framework initialized
[ 0.089677] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089686] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.095225] CPU: Testing write buffer coherency: ok
[ 0.095557] Setting up static identity map for 0x805dd470 - 0x805dd4c8
[ 0.096339] devtmpfs: initialized
[ 0.097828] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.103583] omap_hwmod: tptc0 using broken dt data from edma
[ 0.103651] omap_hwmod: tptc1 using broken dt data from edma
[ 0.103709] omap_hwmod: tptc2 using broken dt data from edma
[ 0.107641] omap_hwmod: debugss: _wait_target_disable failed
[ 0.162169] pinctrl core: initialized pinctrl subsystem
[ 0.163019] regulator-dummy: no parameters
[ 0.165004] NET: Registered protocol family 16
[ 0.166651] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.168727] cpuidle: using governor ladder
[ 0.168741] cpuidle: using governor menu
[ 0.173893] syscon 44e10000.control_module: regmap [mem 0x44e10000-0x44e107fb] registered
[ 0.175085] platform 49000000.edma: alias fck already exists
[ 0.175104] platform 49000000.edma: alias fck already exists
[ 0.175115] platform 49000000.edma: alias fck already exists
[ 0.176030] OMAP GPIO hardware version 0.1
[ 0.186896] No ATAGs?
[ 0.186916] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.207855] bio: create slab <bio-0> at 0
[ 0.220661] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.221480] vmmcsd_fixed: 3300 mV
[ 0.223883] vgaarb: loaded
[ 0.224304] i2c-core: driver [palmas] using legacy suspend method
[ 0.224313] i2c-core: driver [palmas] using legacy resume method
[ 0.224888] SCSI subsystem initialized
[ 0.226091] usbcore: registered new interface driver usbfs
[ 0.226245] usbcore: registered new interface driver hub
[ 0.226409] usbcore: registered new device driver usb
[ 0.227217] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c0_pins, deferring probe
[ 0.227240] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral
[ 0.227557] pps_core: LinuxPPS API ver. 1 registered
[ 0.227566] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.227666] PTP clock support registered
[ 0.229245] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.230059] Advanced Linux Sound Architecture Driver Initialized.
[ 0.231392] Switched to clocksource timer1
[ 0.246984] NET: Registered protocol family 2
[ 0.247701] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.247750] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.247787] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.247843] TCP: reno registered
[ 0.247853] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.247868] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.248018] NET: Registered protocol family 1
[ 0.248353] RPC: Registered named UNIX socket transport module.
[ 0.248364] RPC: Registered udp transport module.
[ 0.248369] RPC: Registered tcp transport module.
[ 0.248374] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.249274] hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available
[ 0.251604] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.388499] VFS: Disk quotas dquot_6.5.2
[ 0.388558] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.388988] NFS: Registering the id_resolver key type
[ 0.389054] Key type id_resolver registered
[ 0.389061] Key type id_legacy registered
[ 0.389090] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.389237] msgmni has been set to 995
[ 0.390408] NET: Registered protocol family 38
[ 0.390443] io scheduler noop registered
[ 0.390450] io scheduler deadline registered
[ 0.390474] io scheduler cfq registered (default)
[ 0.391999] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.396552] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.400889] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) is a 8250
[ 1.023529] console [ttyS0] enabled
[ 1.028553] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 1.035583] [drm] Initialized drm 1.1.0 20060810
[ 1.048816] brd: module loaded
[ 1.056362] loop: module loaded
[ 1.059854] (hci_tty): inside hci_tty_init
[ 1.064398] (hci_tty): allocated 250, 0
[ 1.070648] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.080204] usbcore: registered new interface driver asix
[ 1.085829] usbcore: registered new interface driver ax88179_178a
[ 1.092113] usbcore: registered new interface driver cdc_ether
[ 1.098141] usbcore: registered new interface driver smsc95xx
[ 1.104041] usbcore: registered new interface driver net1080
[ 1.109867] usbcore: registered new interface driver cdc_subset
[ 1.115932] usbcore: registered new interface driver zaurus
[ 1.121729] usbcore: registered new interface driver cdc_ncm
[ 1.127848] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.134432] ehci-pci: EHCI PCI platform driver
[ 1.139062] ehci-omap: OMAP-EHCI Host Controller driver
[ 1.144719] usbcore: registered new interface driver cdc_wdm
[ 1.150575] usbcore: registered new interface driver usb-storage
[ 1.157499] mousedev: PS/2 mouse device common for all mice
[ 1.164686] i2c-core: driver [rtc-ds1307] using legacy suspend method
[ 1.171158] i2c-core: driver [rtc-ds1307] using legacy resume method
[ 1.178289] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ 1.186116] i2c /dev entries driver
[ 1.189753] Driver for 1-wire Dallas network protocol.
[ 1.196998] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.283485] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.289780] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 1.296777] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 1.303845] usbcore: registered new interface driver usbhid
[ 1.309444] usbhid: USB HID core driver
[ 1.313573] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 1.323772] oprofile: using arm/armv7
[ 1.327790] TCP: cubic registered
[ 1.331136] Initializing XFRM netlink socket
[ 1.335499] NET: Registered protocol family 17
[ 1.339999] NET: Registered protocol family 15
[ 1.344614] Key type dns_resolver registered
[ 1.349049] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 1.357698] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
[ 1.366475] cpu cpu0: cpu0 clock notifier not ready, retry
[ 1.372104] platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
[ 1.379639] mmc0: new high speed SDHC card at address aaaa
[ 1.385765] PM: bootloader does not support rtc-only!
[ 1.390849] ThumbEE CPU extension supported.
[ 1.395788] mmcblk0: mmc0:aaaa SC16G 14.8 GiB
[ 1.400972] Registering SWP/SWPB emulation handler
[ 1.405957] mmcblk0: p1 p2
[ 1.411057] regulator-dummy: disabling
[ 1.418664] Error: Driver 'tfp410' is already registered, aborting...
[ 1.425483] slave hdmi: could not get i2c
[ 1.429597] platform hdmi: Driver slave requests probe deferral
[ 1.436196] platform 4830e000.lcdc: Driver tilcdc requests probe deferral
[ 1.447327] DCDC1: at 1500 mV
[ 1.451432] vdd_mpu: 925 <--> 1375 mV at 1325 mV
[ 1.457131] vdd_core: 925 <--> 1150 mV at 1125 mV
[ 1.462902] LDO1: at 1800 mV
[ 1.466825] LDO2: at 3300 mV
[ 1.470740] LDO3: 1800 mV
[ 1.474434] LDO4: at 3300 mV
[ 1.478420] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 1.483812] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.489924] remoteproc0: wkup_m3 is available
[ 1.494424] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 1.503438] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 1.514367] remoteproc0: Direct firmware load failed with error -2
[ 1.520666] remoteproc0: Falling back to user helper
[ 1.525806] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[950000<->1325000]:-22
[ 1.538698] dummy 0-0034: Error -121 writing to cec:0xff
[ 1.544327] tda998x 0-0070: Error -121 writing to REG_CURPAGE
[ 1.550152] tda998x 0-0070: Error -121 reading from 0xa
[ 1.555462] tda998x 0-0070: Error -121 writing to 0xa
[ 1.611449] tda998x 0-0070: Error -121 reading from 0xa
[ 1.616741] tda998x 0-0070: Error -121 writing to 0xa
[ 1.681446] tda998x 0-0070: Error -121 reading from 0x1
[ 1.686737] tda998x 0-0070: Error -121 writing to 0x1
[ 1.691864] tda998x 0-0070: Error -121 reading from 0x1
[ 1.697155] tda998x 0-0070: Error -121 writing to 0x1
[ 1.702281] tda998x 0-0070: Error -121 writing to REG_CURPAGE
[ 1.708095] tda998x 0-0070: Error -121 writing to 0x200
[ 1.713396] tda998x 0-0070: Error -121 writing to 0x201
[ 1.718686] tda998x 0-0070: Error -121 writing to 0x202
[ 1.723987] tda998x 0-0070: Error -121 writing to 0x203
[ 1.729278] tda998x 0-0070: Error -121 writing to 0x204
[ 1.734578] tda998x 0-0070: Error -121 writing to 0x205
[ 1.739868] tda998x 0-0070: Error -121 writing to 0x20e
[ 1.745169] tda998x 0-0070: Error -121 writing to 0x211
[ 1.750459] tda998x 0-0070: Error -121 writing to 0x207
[ 1.755759] tda998x 0-0070: Error -121 writing to 0x208
[ 1.761049] tda998x 0-0070: Error -121 writing to 0x209
[ 1.766350] tda998x 0-0070: Error -121 writing to 0x20a
[ 1.771650] tda998x 0-0070: Error -121 writing to 0x206
[ 1.776940] tda998x 0-0070: Error -121 writing to REG_CURPAGE
[ 1.782763] tda998x 0-0070: Error -121 writing to 0x27
[ 1.787966] tda998x 0-0070: Error -121 reading from 0x0
[ 1.793267] tda998x 0-0070: Error -121 reading from 0x2
[ 1.798907] tilcdc 4830e000.lcdc: no encoders/connectors found
[ 1.804835] tilcdc 4830e000.lcdc: failed to initialize mode setting
[ 1.812533] pinctrl-single 44e10800.pinmux: pin 44e10854.0 already requested by leds; cannot claim for 4a100000.ethernet
[ 1.823504] pinctrl-single 44e10800.pinmux: pin-21 (4a100000.ethernet) status -22
[ 1.831020] pinctrl-single 44e10800.pinmux: could not request pin 21 (44e10854.0) from group cpsw_default on device pinctrl-single
[ 1.842916] cpsw 4a100000.ethernet: Error applying setting, reverse things back
[ 1.911456] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.917593] davinci_mdio 4a101000.mdio: detected phy mask ffffffcf
[ 1.925250] libphy: 4a101000.mdio: probed
[ 1.929292] davinci_mdio 4a101000.mdio: phy[4]: device 4a101000.mdio:04, driver Atheros 8031 ethernet
[ 1.938592] davinci_mdio 4a101000.mdio: phy[5]: device 4a101000.mdio:05, driver Atheros 8031 ethernet
[ 1.948737] cpsw 4a100000.ethernet: Detected MACID = 2c:6b:7d:4e:99:bb
[ 1.956660] cpsw 4a100000.ethernet: cpsw: Detected MACID = 2c:6b:7d:4e:99:bd
[ 1.965416] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[ 1.977369] ALSA device list:
[ 1.980368] No soundcards found.
[ 1.989698] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem
[ 1.997105] EXT4-fs (mmcblk0p2): write access will be enabled during recovery
[ 2.184617] EXT4-fs (mmcblk0p2): recovery complete
[ 2.191369] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.199604] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
[ 2.211937] devtmpfs: mounted
[ 2.215367] Freeing unused kernel memory: 260K (c07fa000 - c083b000)
INIT: version 2.88 booting
Error opening /dev/fb0: No such file or directory
Starting udev
[ 2.982115] udevd[852]: starting version 182
[ 3.398243] 47401300.usb-phy supply vcc not found, using dummy regulator
[ 3.532869] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 3.745598] EXT4-fs (mmcblk0p2): re-mounted. Opts: data=ordered
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
[ 4.128474] remoteproc0: powering up wkup_m3
[ 4.156085] remoteproc0: Booting fw image am335x-pm-firmware.elf, size 154412
[ 4.244232] PM: CM3 Firmware Version = 0x190
[ 4.280749] random: dd urandom read with 97 bits of entropy available
[ 4.314125] remoteproc0: remote processor wkup_m3 is now up
[ 4.400820] davinci_evm sound: hdmi-hifi <-> 48038000.mcasp mapping ok
[ 5.419783] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 5.714741] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 1
[ 5.805050] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 5.811952] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 5.819206] usb usb1: Product: MUSB HDRC host driver
[ 5.824202] usb usb1: Manufacturer: Linux 3.14.43-g875c69b musb-hcd
[ 5.830493] usb usb1: SerialNumber: musb-hdrc.1.auto
[ 5.884271] random: nonblocking pool is initialized
[ 5.986625] hub 1-0:1.0: USB hub found
[ 6.002655] hub 1-0:1.0: 1 port detected
[ 6.208397] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
udevadm settle - timeout of 3 seconds reached, the event queue contains:
/sys/devices/ocp/48060000.mmc/mmc_host/mmc0/mmc0:aaaa/block/mmcblk0/mmcblk0p1 (809)
/sys/devices/ocp/48060000.mmc/mmc_host/mmc0/mmc0:aaaa/block/mmcblk0/mmcblk0p2 (810)
ALSA: Restoring mixer settings...
No state is present for card Black
Found hardware: "TI_BeagleBone_B" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card Black
Mon Jul 6 21:02:00 UTC 2015
INIT: Entering runlevel: 5
Configuring network interfaces... [ 7.024971] net eth0: initializing cpsw version 1.12 (0)
[ 7.111919] net eth0: phy found : id is : 0x4dd074
udhcpc (v1.22.1) started
Sending discover...
[ 10.112295] libphy: 4a101000.mdio:04 - Link is Up - 100/Full
Sending discover...
Sending discover...
No lease, forking to background
done.
Starting system message bus: dbus.
UIM SYSFS Node Not Found
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting rpcbind daemon...rpcbind: cannot create socket for udp6
rpcbind: cannot create socket for tcp6
done.
creating NFS state directory: done
starting statd: done
Starting syslogd/klogd: done
Starting thttpd.
Starting Lighttpd Web Server: lighttpd.
2015-07-06 21:02:11: (/home/gtbldadm/ti/oe-layersetup/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa8t2hf-vfp-neon-linux-gnueabi/lighttpd/1.4.33-r1/lighttpd-1.4.33/src/log.c.166) server started
/
Starting Matrix GUI application.
Enabling thermal zones...
/etc/rc5.d/S98thermal-zone-init: line 7: /sys/class/thermal/thermal_zone*/mode: No such file or directory
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
autoconf
binutils
cpp-symlinks
cpp
g++-symlinks
g++
gcc-symlinks
gcc
gdbserver
gstreamer1.0-libav
libgmp10
libmpc3
libmpfr4
make
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
Stopping Bootlog daemon: bootlogd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm /dev/ttyO0
Arago 2015.05 am335x-evm /dev/ttyO0
am335x-evm login:
------------------------------------------------------------------------------------------------------------------
目前遇到的问题是无法ping通pc机,硬件方面的问题可以排除掉,想问我在软件配置方面有没有问题?
期待您的回复,谢谢!