SDK7.01
........................................
........................................
status = app_init_pyramid2(obj->context, &obj->pyramidObj_x3cL, "pyramidObj_x3cL",obj->sensorObj_x3c.num_cameras_enabled);
APP_ASSERT(status == VX_SUCCESS);
status = app_init_pyramid2(obj->context, &obj->pyramidObj_ar143, "pyramidObj_ar143",obj->sensorObj_ar143.num_cameras_enabled);
APP_ASSERT(status == VX_SUCCESS);
........................................
........................................
status = app_create_graph_pyramid2(obj->graph, &obj->pyramidObj_x3cL,obj->scalerObj_x3ca.output1.arr);
APP_ASSERT(status == VX_SUCCESS);
vxRegisterAutoAging(obj->graph, obj->pyramidObj_x3cL.pyramid_delay);
status = app_create_graph_pyramid2(obj->graph, &obj->pyramidObj_ar143,obj->scalerObj_ar143.output1.arr);
APP_ASSERT(status == VX_SUCCESS);
vxRegisterAutoAging(obj->graph, obj->pyramidObj_ar143.pyramid_delay);
35.815407 s: VX_ZONE_ERROR:[ownContextSendCmd:782] Command ack message returned failure cmd_status: -7
35.815414 s: VX_ZONE_ERROR:[ownContextSendCmd:818] tivxEventWait() failed.
35.815477 s: VX_ZONE_ERROR:[ownNodeKernelInit:526] Target kernel, TIVX_CMD_NODE_CREATE failed
35.815480 s: VX_ZONE_ERROR:[ownNodeKernelInit:527] Please be sure the target callbacks have been registered for this core
35.815482 s: VX_ZONE_ERROR:[ownNodeKernelInit:528] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
35.815654 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 16, kernel com.ti.hwa.vpac_msc_pyramid ... failed !!!
35.815672 s: VX_ZONE_ERROR:[vxVerifyGraph:2010] Node kernel init failed
35.815675 s: VX_ZONE_ERROR:[vxVerifyGraph:2064] Graph verify failed
35.831049 s: VX_ZONE_ERROR:[tivxNodeSendCommandTimed:277] vxVerifyGraph should be called before tivxNodeSendCommand can be called on a node in the same graph