Hi Sir
請問AM3352的SDIO最快的DATA RATE為多少?
謝謝
Daniel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
高达 48MHz 的数据传输速率.
详细请阅读TRM 18.1.1 MMCHS Features
www.ti.com.cn/.../spruh73q.pdf
– up to 384Mbit/sec (48MByte/sec) in MMC mode 8-bit data transfer
– up to 192Mbit/sec (24MByte/sec) in High-Speed SD mode 4-bit data transfer
– up to 24Mbit/sec (3MByte/sec) in Default SD mode 1-bit data transfer