This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5729: 使用 phy DP83867IRRGZ ,无法ping通网线直连的设备

Part Number: AM5729


我们公司使用的 am5729,公司自己制作的板子,使用 phy DP83867IRRGZ ,用网线直连同样的am5729板,无法Ping通,但是板子用网线连上交换机,能ping通

问题:1. 是什么原因导致网线直连两台设备无法ping通呢

           2. 有什么解决方法吗

  • 请贴出您使用的SDK,并且详细描述一下两块板子直连是如何ping的。

  • SDK版本为 5.03,系统为 premmpt rt linux,两块板子的ip为同一网段,在板子进入Linux系统后,使用ping命令

  • 请贴出以下指令的结果以及ping命令的信息,我需要咨询相关工程师再给您回复。

    ethtool eth0/eth1

    ethtool -S eth0/eth1

  • # ethtool eth0
    Settings for eth0:
    Supported ports: [ TP MII ]
    Supported link modes: 10baseT/Half 10baseT/Full
    100baseT/Half 100baseT/Full
    1000baseT/Half 1000baseT/Full
    Supported pause frame use: Symmetric Receive-only
    Supports auto-negotiation: Yes
    Supported FEC modes: Not reported
    Advertised link modes: 10baseT/Half 10baseT/Full
    100baseT/Half 100baseT/Full
    [10380.787720] cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
    1000baseT/Half 1000baseT/Full
    Advertised pause frame use: [10380.802954] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    No
    Advertised auto-negotiation: Yes
    Advertised FEC modes: Not reported
    Link partner advertised link modes: 10baseT/Half 10baseT/Full
    100baseT/Half 100baseT/Full
    1000baseT/Full
    Link partner advertised pause frame use: No
    Link partner advertised auto-negotiation: Yes
    Link partner advertised FEC modes: Not reported
    Speed: 1000Mb/s
    Duplex: Full
    Port: MII
    PHYAD: 0
    Transceiver: internal
    Auto-negotiation: on
    Supports Wake-on: d
    Wake-on: d
    Current message level: 0x00000000 (0)

    Link detected: no

  • 板子网口为千兆网口,直连一台百兆网口的设备ping不通,直连另一个千兆网口是能ping通的