我想使用AM335x的CPSW的 ALE交换机功能,A设备连接335X的0端口 B设备连接335X的1端口,然后把335X配置成交换机模式,A设备的网络通过 335X可以访问B设备网络,直接是通过335X的MAC层转发数据,我看到芯片手册上说明的是 2 port switch功能。 请问335X有这样的功能吗?哪里这样的配置例程。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请阅读:
Switch Configuration Interface
dual emac模式是port1和port2两个独立的网口。
switch模式可通过mac内部交换数据包,通常port1和port2处于同一个网段。
如何配置请阅读上一条的回复。