你好,我在用自己做的6678板子时,跑的是网口的GE程序,自己的板子和官方评估版的区别就只是参考时钟和选用的SGMII端口不一样,在跑程序时PSC模块的开启和关闭会有错误。
[C66xx_0] JTAG ID= 0x1009e02f. This is C6678/TCI6608 device, version variant = 1.
DEVSTAT= 0x0000960d. little endian, SPI boot, PLL configuration implies the input clock for core is bypassed.
SmartReflex VID= 60, required core voltage= 1.084V.
Die ID= 0x08009004, 0x04046451, 0x00000000, 0x26ba0021
Device speed grade = 1000MHz.
Enable Exception handling...
Initialize DSP main clock = 100.00MHz/1x10 = 1000MHz
Initialize PASS PLL clock = 100.00MHz/2x21 = 1050.000MHz
GE 1000M fullduplex two DSPs test (DSP0 -> DSP1)...
Disable power domain 2 timeout!
Enable power domain 2 timeout!
Enable power domain 2 timeout!