你好,
目前系统跑的linux,文件系统放在emmc上, 后续想放文件系统到nand, 想问下AM437x 最大支持多大容量的NAND Flash呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
目前系统跑的linux,文件系统放在emmc上, 后续想放文件系统到nand, 想问下AM437x 最大支持多大容量的NAND Flash呢?
对nand flash的最大容量没有要求,但是要使用ROM bootloader支持的nand flash,请参考TRM。
5.2.6.4.2.3 Device Detection and Parameters
https://www.ti.com/lit/ug/spruhl7i/spruhl7i.pdf
谢谢,我们现在用了一款nand,但是内核里面 elm识别不了提示 elm: unsupported config ecc-step=16 ,请帮忙看下是什么问题呢?
31676] nand: device found, Manufacturer ID: 0xad, Chip ID: 0xde
[ 1.638400] nand: Hynix H27UCG8T2ATR-BC 64G 3.3V 8-bit
[ 1.643879] nand: 8192 MiB, MLC, erase size: 2048 KiB, page size: 8192, OOB size: 640
[ 1.652220] using OMAP_ECC_BCH16_CODE_HW ECC scheme
[ 1.657388] omap-elm 48080000.elm: unsupported config ecc-step=16
[ 1.663890] omap2-nand: probe of 8000000.nand failed with error -22
[ 1.710994] omap_i2c 44e0b000.i2c: bus 0 rev0.12 at 100 kHz
[ 1.718655] omap_i2c 4802a000.i2c: bus 1 rev0.12 at 100 kHz