This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am3359中断问题求专家解释-------

我在学习中断的时候,遇到问题:

  AM335X_Software

static void CopyVectorTable(void)
{
    unsigned int *dest = (unsigned int *)AM335X_VECTOR_BASE;
    unsigned int *src =  (unsigned int *)vecTbl;
    unsigned int count;
 
    CP15VectorBaseAddrSet(AM335X_VECTOR_BASE);

    for(count = 0; count < sizeof(vecTbl)/sizeof(vecTbl[0]); count++)
    {
        dest[count] = src[count];
    }
}

const unsigned int AM335X_VECTOR_BASE = 0x4030FC00;

static unsigned int const vecTbl[14]=
{
    0xE59FF018,    /* Opcode for loading PC with the contents of [PC + 0x18] */
    0xE59FF018,    /* Opcode for loading PC with the contents of [PC + 0x18] */
    0xE59FF018,    /* Opcode for loading PC with the contents of [PC + 0x18] */
    0xE59FF018,    /* Opcode for loading PC with the contents of [PC + 0x18] */
    0xE59FF014,    /* Opcode for loading PC with the contents of [PC + 0x14] */
    0xE24FF008,    /* Opcode for loading PC with (PC - 8) (eq. to while(1)) */
    0xE59FF010,    /* Opcode for loading PC with the contents of [PC + 0x10] */
    0xE59FF010,    /* Opcode for loading PC with the contents of [PC + 0x10] */
    (unsigned int)Entry,
    (unsigned int)UndefInstHandler,
    (unsigned int)SVCHandler,
    (unsigned int)AbortHandler,
    (unsigned int)IRQHandler,
    (unsigned int)FIQHandler
};

上面的代码是把 vecTbl[14]  copy到向量入口地0x4030FC00。

问题 1: 假如发生IRQ中断,PC指针是不是等于:0x4030FC00 + 0x18, 从这里取指令?

       如果是,那么这个   0xE24FF008, 是什么意思?

    TI的文档或ARM有没有文档说明这个值是什么?

问题2: 从上面的vecTbl表中,我很容易看成,中断来了,PC是从  (unsigned int)IRQHandler取指,然后跑到这个函数上去。但是,TI的 starterWare为什么要加上前面那一堆数字让人难理解呢?

求解释!!!!!!!   或指出在什么地方可以查到资料.

 

  • 你看看arm的technical reference manual, CP15里面有寄存配置中断向量的入口地址的

  • When an exception branches to the Monitor mode, the core branches to address:
    Monitor_Base_Address + Exception_Vector_Address.
           内存地址           指令
    0x4030FC00:    0xE59FF018,
    0x4030FC04:    0xE59FF018,
    0x4030FC08:    0xE59FF018,
    0x4030FC0c:    0xE59FF018,
    0x4030FC10:    0xE59FF014,
    0x4030FC14:    0xE24FF008,
    0x4030FC18:    0xE59FF010,
    0x4030FC1c:    0xE59FF010,
    0x4030FC20:    (unsigned int)Entry,
    0x4030FC24:    (unsigned int)UndefInstHandler,
    0x4030FC28:    (unsigned int)SVCHandler,
    0x4030FC2c:    (unsigned int)AbortHandler,
    0x4030FC30:    (unsigned int)IRQHandler,
    0x4030FC34:    (unsigned int)FIQHandler

    当IRQ中断来的时候,PC = 0x4030FC18,    ARM 取到指令:0xE59FF010  这个值,会去干什么呢(进行什么操作?)

    我想问的是:  0xE59FF018   0xE59FF010   0xE24FF008 等,这些值是干什么的,一直搞不明白。。。。。

     

     

     

  • 这些都是机器码,会对应一些指令,也就是对PC load的一些指令,你可以用仿真器跟进去看看,最后回到各种异常模式的处理里面去