开始学习c6678,使用自制的板子进行调试。
使用的仿真器是560V2,在ccxml中给0核配置了gel文件,Test connection成功通过。
但是在连接成功后的System Reset过程出错。
failed system restart: ERROR -1183 @ 0x7B No device bus slots available to service the request.Upgrade this request to high priority to force the device to generate a bus slot to service the request.Note that this would be instrusive to your program
距离上一次使用这块板子出的错是出现一堆寄存器的値,,instruction fetch exception,在论坛已经看到建议解决方法是使用ROV检查堆栈,加大堆栈大小。