Other Parts Discussed in Thread: TVP5158
在DM8168+TVP5158平台下,使用DVRRDK-04.01.00.02。当拔掉TVP5158任意一摄像头时,被拔掉的通道依然可以采集到数据,显示器对应通道画面会变成全黑颜色。但如何能让A8核心也知道,TVP5158当前哪个通道的摄像头无连接。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在DM8168+TVP5158平台下,使用DVRRDK-04.01.00.02。当拔掉TVP5158任意一摄像头时,被拔掉的通道依然可以采集到数据,显示器对应通道画面会变成全黑颜色。但如何能让A8核心也知道,TVP5158当前哪个通道的摄像头无连接。
你好,
我在TVP5158的数据手册里,没有找个每个通道同步相关的寄存器,只有整体的。
Subaddress 00h
Lost lock detect
0 No lost lock since this bit was last cleared
1 Lost lock since this bit was last cleared
Color subcarrier lock status
0 Color subcarrier is not locked
1 Color subcarrier is locked
Vertical sync lock status
0 Vertical sync is not locked
1 Vertical sync is locked
Horizontal sync lock status
0 Horizontal sync is not locked
1 Horizontal sync is locked
A8核能否获取到VPSS M3核检测TVP5158是否采集到视频数据信息么?
你好,
TVP5158在没有视频输入的时候,仍然会输出黑屏,所以VPSS M3还是会采集到数据。你能在VPSS M3里添加代码来判断收到的数据是否为黑屏数据么?我没有想到其他更简洁的方法。
Thanks,
Chris