This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我已在ti-linux-kernel (branch=ti-rt-linux-5.4.y ; commit=3be7c8fa970782c88c2a188f7310ccc7256121f7) drivers/net/ethernet/ti/cpsw.c 驱动器的 Git 存储库中实施了 Phy 环回模式自检过程。它目前在我的 am5718-idk 板上工作,具有两个 cpsw 接口(gmac 配置为双 gmac 模式)。
目前我有以下限制:
如果您有兴趣,我可以为您提供补丁以供审核,并且(当然,如果它足够好)在内核中集成。
下面是补丁:
From 7526fa471a712cfd783edcd0bcc97a4ec62a4f41 Mon Sep 17 00:00:00 2001 From: Kamel Hacene <kamel.hacene@safrangroup.com> Date: Mon, 7 Jun 2021 08:13:47 +0000 Subject: [PATCH] net: ethernet: ti: Add phy loopback ethtool self-test for cpsw driver --- drivers/net/ethernet/ti/cpsw.c | 3 +- drivers/net/ethernet/ti/cpsw_ethtool.c | 339 ++++++++++++++++++++++++++++++++ drivers/net/ethernet/ti/cpsw_priv.h | 9 + drivers/net/ethernet/ti/davinci_cpdma.c | 10 + drivers/net/ethernet/ti/davinci_cpdma.h | 2 + 5 files changed, 362 insertions(+), 1 deletion(-) diff --git a/drivers/net/ethernet/ti/cpsw.c b/drivers/net/ethernet/ti/cpsw.c index 5146685eddd8..8544bb193b71 100644 --- a/drivers/net/ethernet/ti/cpsw.c +++ b/drivers/net/ethernet/ti/cpsw.c @@ -1058,7 +1058,7 @@ static void cpsw_fifo_shp_on(struct cpsw_priv *priv, int fifo, int on) writel_relaxed(val, &cpsw->regs->ptype); } -static void _cpsw_adjust_link(struct cpsw_slave *slave, +void _cpsw_adjust_link(struct cpsw_slave *slave, struct cpsw_priv *priv, bool *link) { struct phy_device *phy = slave->phy; @@ -2497,6 +2497,7 @@ static const struct ethtool_ops cpsw_ethtool_ops = { .nway_reset = cpsw_nway_reset, .get_ringparam = cpsw_get_ringparam, .set_ringparam = cpsw_set_ringparam, + .self_test = cpsw_self_test, }; static int cpsw_probe_dt(struct cpsw_platform_data *data, diff --git a/drivers/net/ethernet/ti/cpsw_ethtool.c b/drivers/net/ethernet/ti/cpsw_ethtool.c index 31248a6cc642..843d3f1ad321 100644 --- a/drivers/net/ethernet/ti/cpsw_ethtool.c +++ b/drivers/net/ethernet/ti/cpsw_ethtool.c @@ -16,11 +16,23 @@ #include <linux/skbuff.h> #include "cpsw.h" +#include "cpsw_sl.h" #include "cpts.h" #include "cpsw_ale.h" #include "cpsw_priv.h" #include "davinci_cpdma.h" +#define CPSW_XMETA_OFFSET ALIGN(sizeof(struct xdp_frame), sizeof(long)) +struct __aligned(sizeof(long)) cpsw_meta_xdp { + struct net_device *ndev; + int ch; +}; +#define CPSW_HEADROOM_NA (max(XDP_PACKET_HEADROOM, NET_SKB_PAD) + NET_IP_ALIGN) +#define CPSW_HEADROOM ALIGN(CPSW_HEADROOM_NA, sizeof(long)) + +#define TST_FRAME_SIZE 512 +#define TST_PATTERN 0xAA + struct cpsw_hw_stats { u32 rxgoodframes; u32 rxbroadcastframes; @@ -217,6 +229,14 @@ int cpsw_set_coalesce(struct net_device *ndev, struct ethtool_coalesce *coal) return 0; } +enum cpsw_diagnostics_result { + TEST_LOOP +}; +static const char cpsw_gstrings_test[][ETH_GSTRING_LEN] = { + [TEST_LOOP] = "Loopback test (offline)" +}; +#define CPSW_TEST_LEN (sizeof(cpsw_gstrings_test) / ETH_GSTRING_LEN) + int cpsw_get_sset_count(struct net_device *ndev, int sset) { struct cpsw_common *cpsw = ndev_to_cpsw(ndev); @@ -226,6 +246,8 @@ int cpsw_get_sset_count(struct net_device *ndev, int sset) return (CPSW_STATS_COMMON_LEN + (cpsw->rx_ch_num + cpsw->tx_ch_num) * CPSW_STATS_CH_LEN); + case ETH_SS_TEST: + return CPSW_TEST_LEN; default: return -EOPNOTSUPP; } @@ -744,3 +766,320 @@ int cpsw_get_ts_info(struct net_device *ndev, struct ethtool_ts_info *info) return 0; } #endif + +static void cpsw_loopback_rx_handler(void *token, int len, int status) +{ + struct page *page = token; + void *pa = page_address(page); + struct cpsw_meta_xdp *xmeta = pa + CPSW_XMETA_OFFSET; + struct cpsw_common *cpsw = ndev_to_cpsw(xmeta->ndev); + struct net_device *ndev = xmeta->ndev; + int port = 0; + unsigned int success = 1; + + struct cpsw_priv *priv; + struct cpsw_test *test; + int i; + unsigned char data; + unsigned char* pointer = pa; + int length; + + /* Dual emac mode ? */ + if (cpsw->data.dual_emac && status >= 0) { + /* Refresh ndev if port is not 0 */ + port = CPDMA_RX_SOURCE_PORT(status); + if (port) + ndev = cpsw->slaves[--port].ndev; + + /* Ignore hw headroom and vlan fields */ + pointer += CPSW_HEADROOM; + pointer += CPSW_RX_VLAN_ENCAP_HDR_SIZE; + length = len - (CPSW_HEADROOM + CPSW_RX_VLAN_ENCAP_HDR_SIZE); + } + else + { + /* Single emac -> Ignore hw headroom only */ + pointer += CPSW_HEADROOM; + length = len - CPSW_HEADROOM; + } + + /* Retrieve slave private structures */ + priv = netdev_priv(ndev); + test = &(priv->test); + + netdev_info(ndev, "Loopback test rx handler call (length:%d, pattern:%#x)\n", length, TST_PATTERN); + + /* (Dual emac) Verify RX port == TX port */ + if(success == 1) + { + if (cpsw->data.dual_emac && status >= 0) { + if (port != test->port) + { + netdev_err(ndev, "Loopback test: Invalid RX port (%d). Expected same as TX port (%d).\n", port, test->port); + success = 0; + } + } + } + + /* Verify frame size is correct */ + if(success == 1) + { + if(length != (TST_FRAME_SIZE - CPSW_HEADROOM)) + { + netdev_err(ndev, "Loopback test: Invalid length %d (expected: %d)\n", length, TST_FRAME_SIZE - CPSW_HEADROOM); + success = 0; + } + } + + /* Verify frame data is correct */ + if(success == 1) + { + for(i = 0; i < length; i++) + { + data = *((unsigned char*)(pointer) + i); + if(data != TST_PATTERN) + { + netdev_err(ndev, "Loopback test : bad data(%d) = %#x. Expected pattern %#x\n", i, data, TST_PATTERN); + success = 0; + } + } + } + + /* Set global result */ + test->success = success; + netdev_info(ndev, "Loopback test rx handler call result: %d\n", success); + + /* Call RX handler to drop the frame to network stack */ + (*test->handler)((void *)token, len, status); +} + +static int cpsw_loopback(struct net_device *ndev) +{ + struct cpsw_priv *priv = netdev_priv(ndev); + struct cpsw_common *cpsw = priv->cpsw; + struct cpsw_test *test = &(priv->test); + struct sk_buff *skb = NULL; + unsigned int frame_size; + struct cpdma_chan *txch; + struct cpdma_chan *rxch; + int ret; + int retry; + int success; + + /* Allocate test skb */ + skb = netdev_alloc_skb(ndev, TST_FRAME_SIZE); + if (!skb) + { + netdev_err(ndev, "Could not allocate socket buffer\n"); + return -1; + } + + /* Fill */ + skb_put(skb, TST_FRAME_SIZE); + frame_size = skb->len; + memset(skb->data, TST_PATTERN, frame_size); + + /* Use txqueue 0 */ + txch = cpsw->txv[0].ch; + rxch = cpsw->rxv[0].ch; + + /* Backup and et RX handler */ + test->handler = cpdma_chan_get_handler(rxch); + cpdma_chan_set_handler(rxch, cpsw_loopback_rx_handler); + + /* Reset TX channel */ + ret = cpdma_chan_stop(txch); + if (unlikely(ret != 0)) { + netdev_err(ndev, "Could not stop tx channel 0\n"); + } + ret = cpdma_chan_start(txch); + if (unlikely(ret != 0)) { + netdev_err(ndev, "Could not start tx channel 0\n"); + } + + skb_tx_timestamp(skb); + + /* Set TX port so we can test it in RX handler */ + test->port = priv->emac_port; + + /* Default succes to false */ + success = 0; + + ret = cpdma_chan_submit(txch, skb, skb->data, skb->len, + priv->emac_port + cpsw->data.dual_emac); + if (unlikely(ret != 0)) { + netdev_err(ndev, "Could not send packet. Err: %x\n", ret); + } + else + { + for(retry = 0; retry < 5; retry++) + { + /* Wait for packet to go from Tx to Rx */ + msleep(200); + + /* Try to read a frame, ret return the number of rode frames. In case + * the value is not 0, it means our RX handler has been called and we + * can retrieve the test result. + */ + ret = cpdma_chan_process(rxch, cpsw->rxv[0].budget); + if(ret != 0) + { + /* Retrieve result */ + success = test->success; + break; + } + + /* Dbg */ + netdev_info(ndev, "Retry:%d ; TXstat:%ld ; RXstat:%ld \n", + retry, ndev->stats.tx_bytes, ndev->stats.rx_bytes); + } + } + + /* Restore RX handler */ + cpdma_chan_set_handler(rxch, test->handler); + + return success; +} + +static int cpsw_loopback_test(struct cpsw_slave *slave) +{ + struct phy_device *phy = slave->phy; + struct net_device *ndev = slave->ndev; + struct cpsw_priv *priv = netdev_priv(ndev); + struct cpsw_common *cpsw = priv->cpsw; + bool link; + int ctrl1000; + int bypass; + int slave_port; + int i; + int success = 0; + int bmcr; + + netdev_info(ndev, "Starting loopback test\n"); + slave_port = cpsw_get_slave_port(slave->slave_num); + + /* Disable CPSW interrupts */ + cpsw_intr_disable(cpsw); + + /* Backup phy BMCR configuration */ + bmcr = phy_read(phy, MII_BMCR); + + /* Set loopback, 1Gbit, full duplex, disable autoneg */ + phy_modify(phy, MII_BMCR, + BMCR_LOOPBACK | BMCR_ANENABLE | BMCR_FULLDPLX | BMCR_SPEED1000 | BMCR_SPEED100, + BMCR_LOOPBACK | 0 | BMCR_FULLDPLX | BMCR_SPEED1000 | 0); + + /* Enable CPSW_SL 1Gbit/Full */ + slave->mac_control = CPSW_SL_CTL_GMII_EN | CPSW_SL_CTL_GIG | CPSW_SL_CTL_FULLDUPLEX; + cpsw_sl_ctl_set(slave->mac_sl, slave->mac_control); + + /* Enable ALE forwarding */ + cpsw_ale_control_set(cpsw->ale, slave_port, + ALE_PORT_STATE, + priv->port_state[slave_port]); + + /* Enable master-slave manual configuration (as slave) */ + ctrl1000 = phy_read(phy, MII_CTRL1000); + phy_modify(phy, MII_CTRL1000, + CTL1000_ENABLE_MASTER | CTL1000_AS_MASTER, + CTL1000_ENABLE_MASTER | 0); + + /* Wait for phy to be up */ + for(i = 0; (i < 10) && !(phy_read(phy, MII_BMSR) & BMSR_LSTATUS); i++) + { + msleep(100); + netdev_info(ndev, "Waiting for phy to be up (BMSR=%#x) (check bit: %d)\n", + phy_read(phy, MII_BMSR), BMSR_LSTATUS); + } + + /* Enable ALE bypass mode */ + bypass = cpsw_ale_control_get(cpsw->ale, 0, ALE_BYPASS); + if(!bypass) + { + cpsw_ale_control_set(cpsw->ale, 0, ALE_BYPASS, 1); + } + + /* Loopback test */ + success = cpsw_loopback(ndev); + + /* Restore ALE bypass */ + if(!bypass) + { + cpsw_ale_control_set(cpsw->ale, 0, ALE_BYPASS, 0); + } + + /* Restore phy BMCR */ + phy_write(phy, MII_BMCR, bmcr); + + /* Restore phy CTRL1000 */ + phy_write(phy, MII_CTRL1000, ctrl1000); + + /* Set back speed/duplex and ALE enable */ + _cpsw_adjust_link(slave, priv, &link); + + /* Enable interrupts */ + cpsw_intr_enable(cpsw); + + return success; +} + +void cpsw_self_test(struct net_device *ndev, + struct ethtool_test *etest, u64 *data) +{ + struct cpsw_priv *priv = netdev_priv(ndev); + struct cpsw_common *cpsw = priv->cpsw; + int slave_no = cpsw_slave_index(cpsw, priv); + bool if_running = netif_running(ndev); + int other_slave = slave_no == 1 ? 0 : 1; + + /* Check requested tests */ + if(etest->flags != ETH_TEST_FL_OFFLINE) + { + netdev_err(ndev, "Only offline tests are supported\n"); + etest->flags |= ETH_TEST_FL_FAILED; + return; + } + + /* Interface needs to be up */ + if(!if_running) + { + dev_open(ndev, NULL); + } + + /* No carrier */ + netif_carrier_off(ndev); + + /* Stop other slave */ + if (cpsw->data.dual_emac) + { + if(netif_running(cpsw->slaves[other_slave].ndev)) + { + dev_close(cpsw->slaves[other_slave].ndev); + } + } + + /* Phy loopback test */ + if (cpsw->slaves[slave_no].phy) + { + data[TEST_LOOP] = cpsw_loopback_test(&cpsw->slaves[slave_no]); + if(0 == data[TEST_LOOP]) + { + etest->flags |= ETH_TEST_FL_FAILED; + } + } + else + { + /* Need a phy for loopback test */ + netdev_err(ndev, "This test requires a phy\n"); + etest->flags |= ETH_TEST_FL_FAILED; + return; + } + + /* Restore carrier */ + netif_carrier_on(ndev); + if (cpsw->data.dual_emac) + { + dev_open(cpsw->slaves[other_slave].ndev, NULL); + } +} + diff --git a/drivers/net/ethernet/ti/cpsw_priv.h b/drivers/net/ethernet/ti/cpsw_priv.h index 665bcaff61e2..d3e7d01134a0 100644 --- a/drivers/net/ethernet/ti/cpsw_priv.h +++ b/drivers/net/ethernet/ti/cpsw_priv.h @@ -350,6 +350,12 @@ struct cpsw_common { struct page_pool *page_pool[CPSW_MAX_QUEUES]; }; +struct cpsw_test { + u32 success; + u32 port; + cpdma_handler_fn handler; +}; + struct cpsw_priv { struct net_device *ndev; struct device *dev; @@ -365,6 +371,7 @@ struct cpsw_priv { struct bpf_prog *xdp_prog; struct xdp_rxq_info xdp_rxq[CPSW_MAX_QUEUES]; struct xdp_attachment_info xdpi; + struct cpsw_test test; u32 emac_port; struct cpsw_common *cpsw; @@ -434,5 +441,7 @@ int cpsw_set_channels_common(struct net_device *ndev, struct ethtool_channels *chs, cpdma_handler_fn rx_handler); int cpsw_get_ts_info(struct net_device *ndev, struct ethtool_ts_info *info); +void cpsw_self_test(struct net_device *ndev, struct ethtool_test *eth_test, u64 *data); +void _cpsw_adjust_link(struct cpsw_slave *slave, struct cpsw_priv *priv, bool *link); #endif /* DRIVERS_NET_ETHERNET_TI_CPSW_PRIV_H_ */ diff --git a/drivers/net/ethernet/ti/davinci_cpdma.c b/drivers/net/ethernet/ti/davinci_cpdma.c index 6614fa3089b2..0653dfe421c8 100644 --- a/drivers/net/ethernet/ti/davinci_cpdma.c +++ b/drivers/net/ethernet/ti/davinci_cpdma.c @@ -873,6 +873,16 @@ u32 cpdma_chan_get_rate(struct cpdma_chan *ch) return rate; } +cpdma_handler_fn cpdma_chan_get_handler(struct cpdma_chan *ch) +{ + return ch->handler; +} + +void cpdma_chan_set_handler(struct cpdma_chan *ch, cpdma_handler_fn handler) +{ + ch->handler = handler; +} + struct cpdma_chan *cpdma_chan_create(struct cpdma_ctlr *ctlr, int chan_num, cpdma_handler_fn handler, int rx_type) { diff --git a/drivers/net/ethernet/ti/davinci_cpdma.h b/drivers/net/ethernet/ti/davinci_cpdma.h index d3cfe234d16a..b5dd2e68e024 100644 --- a/drivers/net/ethernet/ti/davinci_cpdma.h +++ b/drivers/net/ethernet/ti/davinci_cpdma.h @@ -97,6 +97,8 @@ int cpdma_chan_set_weight(struct cpdma_chan *ch, int weight); int cpdma_chan_set_rate(struct cpdma_chan *ch, u32 rate); u32 cpdma_chan_get_rate(struct cpdma_chan *ch); u32 cpdma_chan_get_min_rate(struct cpdma_ctlr *ctlr); +cpdma_handler_fn cpdma_chan_get_handler(struct cpdma_chan *ch); +void cpdma_chan_set_handler(struct cpdma_chan *ch, cpdma_handler_fn handler); enum cpdma_control { CPDMA_TX_RLIM, /* read-write */ -- 2.11.0
稍微解释一下:
文件 cpsw.c:
- 将回调 cpsw_self_test 添加到 ethtool_ops,以便我们可以通过用户空间中的“ethtool -t <iface>”调用它
- 将 _cpsw_adjust_link 设置为非静态,因此我们可以在 cpsw_ethtool.c 中调用它
文件 davinci_cpdma.c:
- 为处理程序添加 getter/setter。在自动测试期间,我将用包装程序替换 rx 处理程序,以检查接收到的帧是否与发出的帧一致
文件 cpsw_ethtool.c:
- 实现 cpsw_self_test 函数,以执行以下操作:
* 将测试的从接口设置为向上,停止另一个接口(双 EMAC)以防止来自另一个从机的帧干扰测试(在我的测试期间从未发生过,因为我无法 100% 确定这不会发生)。
* 禁用中断
* 在 phy BMCR 寄存器中设置 phy 环回模式、1Gbit、全双工(不带自动协商)
* 启用 cpsw_sl 1Gbit/全
* 启用 ALE 转发
* 在 phy MII_CTRL1000 寄存器中启用主/从
* 启用 ALE 旁路
* 用图案填充缓冲器 (0xAA)
* 替换 RX 处理器
* 复位 TX 通道
* 发送帧
// 在这里,RX 处理程序应该接收帧。它会先检查帧的大小和数据,然后在从器件的私有结构中设置结果
* 等待系统执行 RX 处理程序,然后检索结果。
* 恢复 RX 处理程序、ALE、phy 寄存器...
* 调用 _cpsw_adjust_link 以根据之前的值恢复 phy 配置和 cpsw 旁路模式。
* 恢复载波