This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

谁能帮我解决啊error: unresolved symbols remain



我在编译链接的时候遇到了这个错误,里面的函数都是自己写的。在头文件里面有声明,但是为什么出现这个问题呢?CCS是3.3 板子是omapl138

<Linking>

undefined first referenced
symbol in file
--------- ----------------
block_reorgornize1(char *, int *, int *, int *, int *, int) C:\\ICETEK\\evmomapl138_v1\\tests\\ICETEK\\ram\\src\\Debug\\block_div.obj
bwlabel(int *, int, int, int *) C:\\ICETEK\\evmomapl138_v1\\tests\\ICETEK\\ram\\src\\Debug\\block_div.obj

error: unresolved symbols remain
error: errors encountered during linking; "bishe.out" not built