This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6674: 上电BOOT时间

Part Number: TMS320C6674


你好,我现在使用TMS320C6674和C6678。代码量是1.2MBYTE。需要在上电0.5S之内从FLASH读完代码运行起来。

请问使用I2C+spi或者I2C+EMIFW可以实现0.5S内启动吗?

我目前使用的SPI BOOT,boot参数表在SPI中已经配置,boot引导时钟1GHz的CPU主频,SPI使用54MHz得时钟。使用示波器测量上电时刻SPI的CLK引脚,实际运行时钟与设置时钟一致。由于在上电从FLASH读取代码时间,每个字节每个字节中间间隔时间较长,请问这个字节间隔时间能够改善吗?或者说用那种方式都会有字节间隔时间。

下图是SPI_CLK引脚的上电时钟,每个字节之间间隔时间太长。