This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA821U: J7200 EVM 使用SD Card启动Multi-Image问题

Part Number: DRA821U


为了方便多人同时开发,我们在 j7200_evm BOARD上,尝试用【MMCSD+SBL】的方式启动调试Gateway Demo,结果不是所有核都能正常启动(MCU2_0未启动)。

想确认一下TI目前的Demo是否支持这样的启动方式?如果支持的话,我们的配置文件还有哪些地方需要改进。

【MMCSD+SBL】启动方式:
Boot Mode:MMCSD
Boot File:SBL
tifs:/packages/ti/drv/sciclient/soc/V2/tifs.bin
应用程序:combined.appimage(使用combined_appimage tool生成的多核Image)

生成combined.appimage使用的文件:
can_traffic_generator_app_mcu1_0_release.xer5f
app_remoteswitchcfg_server.xer5f
can_eth_gateway_app_mcu2_1_release.xer5f

参考文档1. ti-processor-sdk-rtos-j7200-evm-07_03_00_07/gateway-demos/docs/Can-Eth-User_Guide.html
参考文档2. ti-processor-sdk-rtos-j7200-evm-07_03_00_07/pdk_j7200_07_03_00_29/docs/userguide/j7200/boot/boot_k3.html#building-the-sbl-and-its-components

  • 能否把boot的log信息发一下?

  • 以下是SBL启动log。

    Opening serial port /dev/ttyUSB5
    115200:8N1:xonxoff=0:rtscts=0
    Program will end in 30 seconds
    Printing timing information for each line
    Skipping check of serial device
    Use Control-C to stop...
    [0.000001 0.000001] SBL Revision: 01.00.10.00 (Aug 3 2021 - 13:41:32)
    [1.149833 1.149832] TIFS ver: 21.5.0--v2021.05 (Terrific Llam
    [1.182115 0.032282] SCISERVER Board Configuration header population... PASSED
    [1.246065 0.063950] Sciclient_setBoardConfigHeader... PASSED
    [1.293969 0.047904] Initlialzing PLLs ...done.
    [1.325900 0.031931] InitlialzingClocks ...done.
    [1.357809 0.031909] Initlialzing DDR ...done.
    [1.437834 0.080025] Initializing GTC ...Begin parsing user application
    [1.485902 0.048068] Calling Sciclient_procBootRequestProcessor, ProcId 0x20...
    [1.549906 0.064004] Calling Sciclient_procBootRequestProcessor, ProcId 0x21...
    [1.613844 0.063938] Calling Sciclient_procBootRequestProcessor, ProcId 0x1...
    [1.662044 0.048200] Calling Sciclient_procBootRequestProcessor, ProcId 0x2...
    [1.726000 0.063956] Calling Sciclient_procBootRequestProcessor, ProcId 0x6...
    [1.789879 0.063879] Calling Sciclient_procBootRequestProcessor, ProcId 0x7...
    [1.917834 0.127955] Searching for X509 certificate ...not found
    [1.965820 0.047986] Switching core id 4, proc_id 0x1 to split mode...
    [2.013907 0.048087] Calling Sciclient_procBootGetProcessorState, ProcId 0x1...
    [2.077937 0.064030] Sciclient_procBootSetProcessorCfg, ProcId 0x1, enabling split mode...
    [2.142112 0.064175] Calling Sciclient_procBootGetProcessorState, ProcId 0x1...
    [2.206078 0.063966] Enabling MCU TCMs after reset for core 4
    [2.253861 0.047783] Disabling HW-based memory init of MCU TCMs for core 4
    [2.302068 0.048207] Sciclient_procBootSetProcessorCfg update TCM enable/disable settings...
    [2.381799 0.079731] Copying 0x40 bytes to 0x41010000
    [2.414058 0.032259] Copying 0x28 bytes to 0x41010100
    [2.446052 0.031994] Copying 0x17700 bytes to 0x41ca1520
    [2.573767 0.127715] Copying 0x6ff8 bytes to 0x41cb8c20
    [2.637764 0.063997] Copying 0x868 bytes to 0x41cc2e00
    [2.670114 0.032350] Copying 0x4f68 bytes to 0x41ce2100
    [2.733788 0.063674] Copying 0x3484 bytes to 0x41ce7068
    [2.781723 0.047935] Copying 0x2c88 bytes to 0x41cea4ec
    [2.829712 0.047989] Copying 0x1700 bytes to 0x41ced180
    [2.861968 0.032256] Copying 0x200 bytes to 0x41cf2900
    [2.894196 0.032228] Copying 0x200 bytes to 0x41cf2b00
    [2.941910 0.047714] Copying 0x200 bytes to 0x41cf2d00
    [2.973934 0.032024] Copying 0x2000 bytes to 0x41cfdb00
    [3.021710 0.047776] Setting entry point for core 4 @0x41010000
    [3.069766 0.048056] Copying 0x5e6d0 bytes to 0x9e800000
    [3.453654 0.383888] Only load (not execute) image @0x9e800000
    [3.501737 0.048083] Copying 0x1005808 bytes to 0x80080000
    [18.844797 15.343060] Only load (not execute) image @0x80080000
    [18.892882 0.048085] Copying 0xad24 bytes to 0x82000000
    [18.972736 0.079854] Only load (not execute) image @0x82000000
    [19.020779 0.048043] Sciclient_pmSetModuleState On, DevId 0x4...
    [19.068740 0.047961] Copying 0x9bf0 bytes to 0x70000000
    [19.132673 0.063933] Setting entry point for core 0 @0x70000000
    [19.180881 0.048208] Sciclient_procBootReleaseProcessor, ProcId 0x20...
    [19.229022 0.048141] Sciclient_procBootReleaseProcessor, ProcId 0x21...
    [19.277016 0.047994] Sciclient_procBootReleaseProcessor, ProcId 0x1...
    [19.340737 0.063721] Sciclient_procBootReleaseProcessor, ProcId 0x2...
    [19.388878 0.048141] Sciclient_procBootReleaseProcessor, ProcId 0x6...
    [19.436905 0.048027] Sciclient_procBootReleaseProcessor, ProcId 0x7...
    [19.484947 0.048042] Calling Sciclient_procBootRequestProcessor, ProcId 0x20...
    [19.548943 0.063996] Sciclient_procBootSetProcessorCfg, ProcId 0x20, EntryPoint 0x70000000...
    [19.628866 0.079923] Sciclient_pmSetModuleClkFreq, DevId 0xca @ 2000000000Hz...
    [19.692659 0.063793] Sciclient_pmSetModuleState Off, DevId 0xca...
    [19.740712 0.048053] Sciclient_pmSetModuleState On, DevId 0xca...
    [19.788713 0.048001] Sciclient_procBootReleaseProcessor, ProcId 0x20...
    [19.836787 0.048074] Calling Sciclient_procBootRequestProcessor, ProcId 0x1...
    [19.900804 0.064017] Sciclient_procBootSetProcessorCfg, ProcId 0x1, EntryPoint 0x41010000...
    [19.964959 0.064155] Sciclient_pmSetModuleClkFreq, DevId 0xfa @ 1000000000Hz...
    [20.028894 0.063935] Copying first 128 bytes from app to MCU ATCM @ 0x0 for core 4
    [20.092885 0.063991] Calling Sciclient_procBootRequestProcessor, ProcId 0x2...
    [20.156757 0.063872] Skipping Sciclient_procBootSetProcessorCfg for ProcId 0x2, EntryPoint 0xfffffffe...
    [20.236881 0.080124] Calling Sciclient_procBootRequestProcessor, ProcId 0x1...
    [20.300801 0.063920] Starting Sciserver..... PASSED
    [20.301716 0.000915] CAN Profile App:Variant - Pre Compile being used !!!
    [20.303255 0.001539] CAN Profile App: Successfully Enabled CAN Transceiver MCU MCAN0!!!
    [20.380724 0.077469] CAN Profile App: Successfully Enabled CAN Transceiver MCU MCAN1!!!

  • Gateway Demos 不支持SD card boot mode. 只支持OSPI和CCS boot mode。

  • 感谢回复:

    我仍有如下两个疑问:

    1、我理解multi-image从SD卡启动和OSPI启动只是启动介质不同罢了,同样的mult-image在OSPI能启动,那么在SD卡不也应该能启动吗?

    2、Gateway Demos 不支持SD card boot mode,是哪个参数决定了不支持SD卡启动呢?