This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
1、 技术要求中有摄像头断开、接入检查,我们以为TVP5158会提供检测寄存器,但是经过详细了解datasheet,其只有1位检测寄存器,而无法同时检测其上4路摄像头的断开与接入。
2、想软件方面进行检测。软件方法参考了:bbs.eeworld.com.cn/thread-464947-1-1.html 想通过M3内核多久没有收到TVP5158数据作为检测点。但是我们目前在第一步编译方面就遇到了问题。我们仅试验了添加Vps_print函数,发现程序可以运行,但是打印无改变。
因此想向您咨询:
1、M3内核程序修改后,我该如何编译和修改。
2、修改后我需要一个标志位,不管是使用通讯,或者是M3写文件然后A8读取、或者其他的方式,只要A8能了解此标志位就可以,您那有什么好办法么。