This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3MV: 关于TDA3MV使用QSPI FLASH BOOT的几个问题

Part Number: TDA3MV


各位:

         大家好,在此请教几个问题,感谢并期待回复。本人第一次围绕TDA3MV平台进行硬件开发,参考了TRM以及TDA3x-15X15 EVM,有个疑问,使用QSPI FLASH进行BOOT,QSPI FLASH最大容量支持多大?

         在TRM中第25.8.4章节写了BOOT QSPI最大容量为128Mbit,但开发板上挂的却是1Gbit的QSPI FLASH,在TDA3x-15X15 EVM的User Guide中3.9.2章节写了该1Gbit的QSPI Flash用于基础的

存储以及BOOT,这两者冲突吗,是不是仅仅使用了(128Mbit/1Gbit)?

         2、BOOT段程序最少需要占据多少存储空间呢?开发板上的64Mb的QSPI FLASH是否也是用于简单程序的引导?