This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM8148: DVRRDK_04.01.00.02

Part Number: TMS320DM8148


我DM8148要使用2g的DDR,有个帖子里面介绍要修改uImage的链接地址,

目前编译出来我看.uImage.cmd文件中的指定的地址是0x80008000, "mkimage -A arm -O linux -T kernel -C none -a 0x80008000 -e 0x80008000 -n 'Linux-2.6.37' -d arch/arm/boot/zImage uImage",

 这个地址在DVRRDK_04.01.00.02开发包中那个文件里面指定的?有人知道吗,我想改成0xc0008000 

"mkimage -A arm -O linux -T kernel -C none -a 0xc0008000 -e 0xc0008000 -n 'Linux-2.6.37' -d arch/arm/boot/zImage uImage",