亲爱的TI官方:
是这样的,我最近在使用TMS32C5535的DSPLIB的时候遇到了一些问题,我在官方下载了“SPRC100-C55_DSPLIB-03.00.00.03-Setup”并且安转,但是我在使用里面提供的“EXAMPLES“例程的时候遇到了以下的编译问题,最近摸索了好久也解决不了。请官方帮我看看解决一下,非常感谢!
**** Clean-only build of configuration Debug for project iir32 ****
"D:\\CCS\\ccs\\utils\\bin\\gmake" -k clean
DEL /F "C:\c55_lp\c55_dsplib_3.00\EXAMPLES\iir32\ccsv5\Debug\iir32.out"
DEL /F "Iir32_t.obj" "TEST.obj"
DEL /F "Iir32_t.d"
DEL /F "TEST.d"
找不到 C:\c55_lp\c55_dsplib_3.00\EXAMPLES\iir32\ccsv5\Debug\iir32.out
找不到 C:\c55_lp\c55_dsplib_3.00\EXAMPLES\iir32\ccsv5\Debug\Iir32_t.obj
找不到 C:\c55_lp\c55_dsplib_3.00\EXAMPLES\iir32\ccsv5\Debug\Iir32_t.d
找不到 C:\c55_lp\c55_dsplib_3.00\EXAMPLES\iir32\ccsv5\Debug\TEST.d
Finished clean
**** Build Finished ****
Buildfile generation error occurred..
Referenced project 'dsplib' does not exist in the workspace. Project 'iir32' may not build as expected.
Build stopped..