Other Parts Discussed in Thread: TMS320C6654
大家好
之前我的UART是通过核发送 比较占用核时间 准备通过EDMA3发送
EDMA3的64个通道是支持UART发送的
但是在这64个通道里没看到SRIO 我原本也想用EDMA3传输SRIO
难道不可以???
看了下SRIO的手册 是不是SRIO的传输本身就是一种DMA?
SRIO和EDMA3是啥关系???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好
之前我的UART是通过核发送 比较占用核时间 准备通过EDMA3发送
EDMA3的64个通道是支持UART发送的
但是在这64个通道里没看到SRIO 我原本也想用EDMA3传输SRIO
难道不可以???
看了下SRIO的手册 是不是SRIO的传输本身就是一种DMA?
SRIO和EDMA3是啥关系???
应该是可以的,请参考datasheet 4.2 Switch Fabric Connections Matrix看一下
SRIO_Master与EDMA3CC/EDMA3TC(0-3)是连通的
The main TeraNet switch fabric (see the device-specific data manual) arbitrates bus requests from all of the masters (like DSP core(s), EMAC, SRIO, etc.) to the shared slave resources (peripherals and memories).
SRIO手册:
LSU setup by EDMA
可通过CIC1 input events events 93 - 116。
Table 7-35 CIC1 Event Inputs (Secondary Events for EDMA3_CC)