我看到所有的AM3359开发板从SD/串口/NANDFLASH启动选项都是通过设置拨码开关实现的,如果我理解不错的话,应该是uboot中会判断连接拨码开关的IO状态然后,选择相应从哪里启动吧?现在,我设计中需要将开发板上的拨码开关的IO作为其他用途,而且我固定只需要从NANDFLASH启动即可,是否应该删除这段代码呢?这段代码在哪里?采用的是你们官方使用的uboot以及相关资料
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我看到所有的AM3359开发板从SD/串口/NANDFLASH启动选项都是通过设置拨码开关实现的,如果我理解不错的话,应该是uboot中会判断连接拨码开关的IO状态然后,选择相应从哪里启动吧?现在,我设计中需要将开发板上的拨码开关的IO作为其他用途,而且我固定只需要从NANDFLASH启动即可,是否应该删除这段代码呢?这段代码在哪里?采用的是你们官方使用的uboot以及相关资料
不是uboot做的判断,是rom code对启动顺序做的判断。
rom code是固化在芯片里面的。
请参考 technical reference manual中的第26章以及我们各种开发板的原理图