This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6657的cvdd引脚连接问题



为了加强对功耗的控制,CVDD可以从0.85V到1.1V动态调整,但外部需要多加几个芯片辅助实现该功能,我的问题是:
可不可以不要这个电压动态调整功能,将CVDD直接固定在1.0V,以降低供电复杂度,减少芯片?
CVDD是不是电压越高,芯片的性能越好,1.1V是不是最好的?