This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

想用AM335X+External Gigabyte PHY来实现一个数据采集传输系统

功能是用外部时钟上升沿触发读取32位GPIO的数据,并将读取到的数据进行TCP封包然后通过千兆以太网发送,不需要任何显示输出。要求能达到200-300Mbps的有效数据传输率(去除以太网传输开销以外的数据传输率,每次持续时间为10分钟左右),通过CAN总线来监控系统工作状态,选用AM335X是否合适,如果合适的话整个系统应该选用什么样的配置(处理器,PHY,电源管理),应该选用哪款开发平台?是否可以采用RTOS?是否需要额外购买IP(需要的话购买IP的费用大概为多少)?如果采用AM335X不合适的话TI这边有什么解决方案可以推荐?

其它信息:设备持续开机时间为3-6个月,DC24V供电,机内无散热风扇但有较大的工作空间