This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: DDR基板延时数据

Part Number: TMS320C6678


TI技术专家您好,C6678的DDR3部分基板管教延时数据能否发一份?同时请问下两个问题:

1.PCB是否需要加管脚延时呢?

2.DDR3初始化不过,我们硬件上边接在PTV15脚上的电阻是1%的44.2Ω,我在其中5块板上配置DDR_TERM为RZQ/6没问题,但是有一块不行,配成RZQ/4就OK了。除了此处电阻还有什么会导致此类现象呢?

谢谢。

  • 1、不需要知道该信息,严格按照TI提供的布线规则即可。

    www.ti.com/.../spracl8.pdf

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/990384/66ak2g12-keystone-ii-66ak2g12aby100-pin-delay-values

    2、除了硬件部分需要严格按照TI手册要求之外,还需要做leveling来优化读写时序。

    www.ti.com.cn/.../sprabl2e.pdf

  • 请问ti工程师,您说的leveling,是指的6678 ddr控制器的硬件自动leveling吗? 像AM335X,需要进行software leveling,是因为此类芯片不支持硬件leveling吗?

  • 请问ti工程师,您说的leveling,是指的6678 ddr控制器的硬件自动leveling吗? 像AM335X,需要进行software leveling,是因为此类芯片不支持硬件leveling吗?

  • software leveling。

    为了保证DDR3的信号完整性,优化相关的读写时序参数,匹配不同板子因板材、layout走线、线宽等多种因素可能会造成的阻抗变化,所以要求,DDR3的设计,必须要进行Software Leveling,获得最适应于当前layout的DDR3 PHY读写参数。

  • 如果叫softleveling的话,还请麻烦再继续解答下我的疑惑:

    根据ti pdk库下提供的示例程序关于ddr3初始化接口:

    void ddr3_setup_auto_lvl_1333()
    {
    //int i,TEMP,startlo, stoplo,starthi, stophi;
    int TEMP;
    KICK0 = KICK0_UNLOCK;
    KICK1 = KICK1_UNLOCK;

    /* Wait for PLL to lock = min 500 ref clock cycles.
    With refclk = 100MHz, = 5000 ns = 5us */
    sleep_timer(1000);

    /***************** 3.2 DDR3 PLL Configuration ************/
    /* Done before */

    /**************** 3.0 Leveling Register Configuration ********************/
    /* Using partial automatic leveling due to errata */

    /**************** 3.3 Leveling register configuration ********************/
    DDR3_CONFIG_REG_0 &= ~(0x007FE000); // clear ctrl_slave_ratio field
    DDR3_CONFIG_REG_0 |= 0x00200000; // set ctrl_slave_ratio to 0x100
    DDR3_CONFIG_REG_12 |= 0x08000000; // Set invert_clkout = 1
    DDR3_CONFIG_REG_0 |= 0xF; // set dll_lock_diff to 15

    //From 4.2.1 Executing Partial Automatic Leveling -- Start
    DDR3_CONFIG_REG_23 |= 0x00000200; //Set bit 9 = 1 to use forced ratio leveling for read DQS
    //From 4.2.1 Executing Partial Automatic Leveling -- End

    //Values with invertclkout = 1
    /**************** 3.3 Partial Automatic Leveling ********************/
    /*DATA0_WRLVL_INIT_RATIO = 0x78;
    DATA1_WRLVL_INIT_RATIO = 0x76;
    DATA2_WRLVL_INIT_RATIO = 0x72;
    DATA3_WRLVL_INIT_RATIO = 0x76;
    DATA4_WRLVL_INIT_RATIO = 0x69;
    DATA5_WRLVL_INIT_RATIO = 0x69;
    DATA6_WRLVL_INIT_RATIO = 0x5B;
    DATA7_WRLVL_INIT_RATIO = 0x60;
    DATA8_WRLVL_INIT_RATIO = 0x00;

    DATA0_GTLVL_INIT_RATIO = 0xAF;
    DATA1_GTLVL_INIT_RATIO = 0xB1;
    DATA2_GTLVL_INIT_RATIO = 0xA3;
    DATA3_GTLVL_INIT_RATIO = 0xA0;
    DATA4_GTLVL_INIT_RATIO = 0x9B;
    DATA5_GTLVL_INIT_RATIO = 0x9B;
    DATA6_GTLVL_INIT_RATIO = 0x98;
    DATA7_GTLVL_INIT_RATIO = 0x92;
    DATA8_GTLVL_INIT_RATIO = 0x00; */

    //Do a PHY reset. Toggle DDR_PHY_CTRL_1 bit 15 0->1->0
    DDR_DDRPHYC &= ~(0x00008000);
    DDR_DDRPHYC |= (0x00008000);
    DDR_DDRPHYC &= ~(0x00008000);

    /***************** 3.4 Basic Controller and DRAM Configuration ************/
    DDR_SDRFC = 0x0000c34; // enable configuration

    /* DDR_SDTIM1 = 0x1113783C; */
    TEMP = 0;
    TEMP |= 0x8 << 25; // T_RP bit field 28:25
    TEMP |= 0x8 << 21; // T_RCD bit field 24:21
    TEMP |= 0x9 << 17; // T_WR bit field 20:17
    TEMP |= 0x17 << 12; // T_RAS bit field 16:12
    TEMP |= 0x20 << 6; // T_RC bit field 11:6
    TEMP |= 0x7 << 3; // T_RRD bit field 5:3
    TEMP |= 0x4; // T_WTR bit field 2:0
    DDR_SDTIM1 = 0x0AAAE4E2; //TEMP;

    /* DDR_SDTIM2 = 0x30717FE3; */
    TEMP = 0;
    TEMP |= 0x3 << 28; // T_XP bit field 30:28
    TEMP |= 0x71 << 16; // T_XSNR bit field 24:16
    TEMP |= 0x1ff << 6; // T_XSRD bit field 15:6
    TEMP |= 0x4 << 3; // T_RTP bit field 5:3
    TEMP |= 0x3; // T_CKE bit field 2:0
    DDR_SDTIM2 = 0x206B7FDA;//TEMP;

    /* DDR_SDTIM3 = 0x559F86AF; */
    TEMP = 0;
    TEMP |= 0x5 << 28; // T_PDLL_UL bit field 31:28 (fixed value)
    TEMP |= 0x5 << 24; // T_CSTA bit field 27:24 (fixed value)
    TEMP |= 0x4 << 21; // T_CKESR bit field 23:21
    TEMP |= 0x3f << 15; // T_ZQCS bit field 20:15
    TEMP |= 0x6a << 4; // T_RFC bit field 12:4
    TEMP |= 0xf; // T_RAS_MAX bit field 3:0 (fixed value)
    DDR_SDTIM3 = 0x557F867F; //TEMP;

    DDR_DDRPHYC = 0x0010010F;

    DDR_ZQCFG = 0x70073214;

    DDR_PMCTL = 0x0;

    DDR_SDRFC = 0x0000c34; // enable configuration

    /* DDR_SDCFG = 0x63062A32; */
    /* New value with DYN_ODT disabled and SDRAM_DRIVE = RZQ/7 //0x63222A32; // last config write DRAM init occurs */
    TEMP = 0;
    TEMP |= 0x3 << 29; // SDRAM_TYPE bit field 31:29 (fixed value)
    TEMP |= 0x0 << 27; // IBANK_POS bit field 28:27
    TEMP |= 0x3 << 24; // DDR_TERM bit field 26:24
    TEMP |= 0x0 << 21; // DYN_ODT bit field 22:21
    TEMP |= 0x1 << 18; // SDRAM_DRIVE bit field 19:18
    TEMP |= 0x2 << 16; // CWL bit field 17:16
    TEMP |= 0x0 << 14; // NM bit field 15:14
    TEMP |= 0xA << 10; // CL bit field 13:10
    TEMP |= 0x4 << 7; // ROWSIZE bit field 9:7
    TEMP |= 0x3 << 4; // IBANK bit field 6:4
    TEMP |= 0x0 << 3; // EBANK bit field 3:3
    TEMP |= 0x2; // PAGESIZE bit field 2:0
    DDR_SDCFG = 0x63072B33;//TEMP;

    //Wait 600us for HW init to complete
    sleep_timer(100000);

    DDR_SDRFC = 0x0000c34; //0x00001450; //Refresh rate = (7.8*666MHz)

    /**************** 4.2.1 Executing Partial Automatic Leveling ********************/

    DDR_RDWR_LVL_RMP_CTRL = 0x80000000; //enable full leveling

    DDR_RDWR_LVL_CTRL = 0x80000000; //Trigger full leveling - This ignores read DQS leveling result and uses ratio forced value

    //(0x34) instead
    //Wait for min 1048576 DDR clock cycles for leveling to complete = 1048576 * 1.5ns = 1572864ns = 1.57ms.
    //Actual time = ~10-15 ms
    sleep_timer(100000);
    //GEL_TextOut("\nDDR3 initialization is complete.\n");
    }

    以上代码  哪一部分是softleveling? 我查阅手册,上序代码中,“4.2.1 Executing Partial Automatic Leveling ”部分是关于硬件leveling的启动;

  • software leveling就是根据前面链接中的表格获取获得最适应于当前layout的DDR3 PHY读写参数,并修改代码中的值。