如题,是不是除了一个是单核,一个是8核,其他的都一样~?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1GHz 的 TMS320C6655 DSP支持多达 128 通道的 G.729AB。C6655 单内核解决方案则分别支持高达 40 GMAC 与 20 GLOPS 以及 27.2 GMAC 与 13.6 GLOPS 的性能。在正常工作情况下,C6655 的功耗数为 2.5W 。
10GHz多核DSP TMS320C6678可实现高性能多媒体解决方案,C6678有8个1.25GHz DSP内核,可在10W功耗下实现160GFLOP的“超高”计算性能。德州仪器中国区通用DSP业务发展经理郑小龙指出:“C6678的性能是任何已推出多核DSP的5倍。TMS320C6678基于TI的Keystone多核架构,采用了可自动调整内核电压的专有SmartReflex技术,因此具有单位MHz/GMAC/GFLOP的最低功耗。除上述特性外,还有众多高速I/O接口,8MB的L2闪存,8GB的L3闪存,及12.8GB/s的存储器带宽。