您好!
TI对于TMS320C6678这个多核DSP推荐的电源方案是什么?除了Hardware Design guide上面说的UCD9222和UCD7242外还有其他的吗?
还有就是,UCD9222和UCD7242这个方案的资料在哪儿下载?Hardware design guide中的原理图看不清楚,也没有BOM,封装信息等。
非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
TI对于TMS320C6678这个多核DSP推荐的电源方案是什么?除了Hardware Design guide上面说的UCD9222和UCD7242外还有其他的吗?
还有就是,UCD9222和UCD7242这个方案的资料在哪儿下载?Hardware design guide中的原理图看不清楚,也没有BOM,封装信息等。
非常感谢!
c66X DSP有两种推荐电源方案,一种是EVM的参考设计,在购买EVM带的光盘中有相应的原理图,网上也有相应的EVM原理图等资料下载:http://www.advantech.com/Support/TI-EVM/
还有一种参考方案是基于TPS56121+LM10010的方案,链接为:http://www.ti.com/tool/pmp7256
谢谢 Andy Yin1
我刚看见advantech的说明,也用C6678_power_consumption_summary计算了下,
advantech用的UCD9222+UCD7242只能用在1GHz,如果想用1.25GHz的,这个电源就不能用了,因为CVDD要大于10A了,请问,如果想用1.25G 的,应该用那种方案呢?
非常感谢!