Part Number: TMS320C6416
请问6416可以从16位的flash中启动吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6416
请问6416可以从16位的flash中启动吗
可以。
Two External Memory Interfaces (EMIFs) − One 64-Bit (EMIFA), One 16-Bit (EMIFB)
您好,我看手册上说 EMIFB 8-bit ROM boot with default timings (default mode),16位的是不是不行了
抱歉造成误解,我重新看了一下 ROM只支持8 bit,以下文档也有说明。
The C64x only supports 8-bit ROM boot, where data should be stored in the endian format that the system is using.