This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TVP5150的一些疑惑

Other Parts Discussed in Thread: TVP5150

关于TVP5150有以下三个pin不知道具体的应用意义。

pin 23 FID/GLCO 不知道其具体的含义,是否一定要接到后端的DSP。是悬空、接地、还是接到机器的VCC

pin 26 AVID 不知道其具体的含义,是否一定要接到后端的DSP。

pin 27输入输出的pin ,是否一定要接到后端的DSP。    

  • 这几个引脚的定义在TVP5150 的datasheet上都有解释,并不是一定要接DSP,电路中FID/GLCO可以通过一2.2Kohm下拉电阻到地。AVID可以直接悬空。pin27也是个多个功能复用,如果不用的话,可以直接通过一10kohm下拉电阻到地。