hi,大家好,我有个关于DSPF_sp_fftSPxSP_cn()函数求fft变换的问题,在文档里面有
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,大家好,我有个关于DSPF_sp_fftSPxSP_cn()函数求fft变换的问题,在文档里面有
看一下例程。
ti-processor-sdk-rtos-c667x-evm-06.03.00.106-Windows\dsplib_c66x_3_4_0_4\examples\fft_sp_ex
非常感谢您的回答,我有读过您的提供的例程,例程里面是定义了一个float x_ref [2*N]; 并对所有奇数位置上都赋给0值(给的虚部为0),因此我猜想这仍然是一个N点的FFT变换,但我不明白的是对于twiddle factors,ptr_w以及 bit reversal coefficients, brev,这两个参数,是否需要我每次在调用时都自己定义,例如,假设我有一个长度为1024个采样点的数列,我需要对这个数列进行FFT变换,在MATLAB中我只需要fft(input_array,1024)就可以了,但是在调用DSP的这个函数上面,我不知道我是否还需要做 1 自己定义一个twiddle factors, 2 定义一个brev。另外对于 int n_min, int offset, int n_max这三个参数,是否没有实际的用途,因我看到这个程序中给出来的是4,0,N, 而在其他地方有看到这个是2,0,N. 能否解释下这三个参数的用法? 非常感谢您的回答!