Other Parts Discussed in Thread: DM3730
开发环境:
DVSDK: ti-dvsdk_dm3730-evm_04_03_00_06,没有做任何修改,只做了一个SD卡启动。
U-Boot:
U-Boot 2010.06 (Dec 22 2011 - 23:11:38)
OMAP34xx/35xx-GP ES2.1, CPU-OPP2 L3-165MHz
OMAP3 EVM board + LPDDR/NAND
I2C: ready
DRAM: 256 MiB
NAND: HW ECC [Kernel/FS layout] selected
512 MiB
*** Warning - bad CRC or NAND, using default environment
In: serial
Out: serial
Err: serial
Read back SMSC id 0x92200000
Die ID #08ee00229ff80000015f26ad0f01e009
Net: smc911x-0
Hit any key to stop autoboot: 0
OMAP3_EVM #
DM3730 EVM(MISTRAL REV G) 是否不支持硬件resize?
根据/ ti-dvsdk_dm3730-evm_04_03_00_06 /psp/UserGuide-04.02.00.07.pdf,是存在resizer硬件的,它具有两种模式:one-shot模式和on-the-fly模式。
根据/ ti-dvsdk_dm3730-evm_04_03_00_06 /psp/ReleaseNotes-04.02.00.07.pdf描述,是不支持ISP-Resizer驱动的。
在\ti-dvsdk_dm3730-evm_04_03_00_06\docs\ dvsdk_4_03_00_06_dm3730_Release_Notes.pdf中,TI修复了一个resize Bug,照理应该对resize有支持的。
在ti-dvsdk_dm3730-evm_04_03_00_06\gstreamer-ti_svnr919\src\Gsttividresize.c中,需要配置#if defined(CONFIG_VIDEO_OMAP34XX_ISP_RESIZER)才能使用resizer硬件,但内核配置文件中没有CONFIG_VIDEO_OMAP34XX_ISP_RESIZER,请问TI支持RESIZER驱动吗?若支持,要如何配置?
在DM3730 MISTRAL REG V开发板下,可以使用TI-gstreamer TIVidResize插件吗?