5509的中断触发方式是什么?电平触发 边沿触发 能不能设置触发方式?怎么设置?在手册里找不到相关说明啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
要求中断信号至少维持两个时钟周期的高电平,然后低电平低至少为3个周期,你说这个信号是下降沿还是上升沿?
Interrupt Timing
The external interrupts (INT[4:0]) are synchronized to the CPU by way of a two-flip-flop synchronizer. The
interrupt inputs are sampled on falling edges of the CPU clock. A sequence of 1-1-0-0-0 on consecutive cycles
on the interrupt pin is required for an interrupt to be detected. Therefore, the minimum low pulse duration on
the external interrupts on the 5509A is three CPU clock periods.