因项目需求正在开发PRU,但PRU只有12KB的指令RAM,所以考虑将代码分到两个PRU单元处理。
但两个PRU单元的数据交互就涉及到共享内存。查看了CMD文件,已有定义段:
/* Specify the System Memory Map */
MEMORY
{
PAGE 0:
PRU_IMEM : org = 0x00000000 len = 0x00003000 /* 12kB PRU Instruction RAM */
PAGE 1:
/* RAM */
PRU_DMEM_0_1 : org = 0x00000000 len = 0x00002000 CREGISTER=24 /* 8kB PRU Data RAM 0_1 */
PRU_DMEM_1_0 : org = 0x00002000 len = 0x00002000 CREGISTER=25 /* 8kB PRU Data RAM 1_0 */
PAGE 2:
PRU_SHAREDMEM : org = 0x00010000 len = 0x00008000 CREGISTER=28 /* 32kB Shared RAM */
...
}
所以在下面的SECTIONS段添加自己的数据到这个段中:
/* Specify the sections allocation into memory */
SECTIONS {
/* Forces _c_int00 to the start of PRU IRAM. Not necessary when */
/* loading an ELF file, but useful when loading a binary */
.text:_c_int00* > 0x0, PAGE 0
.text > PRU_IMEM, PAGE 0
.stack > PRU_DMEM_1_0, PAGE 1
.bss > PRU_DMEM_1_0, PAGE 1
.cio > PRU_DMEM_1_0, PAGE 1
.data > PRU_DMEM_1_0, PAGE 1
.switch > PRU_DMEM_1_0, PAGE 1
.sysmem > PRU_DMEM_1_0, PAGE 1
.cinit > PRU_DMEM_1_0, PAGE 1
.rodata > PRU_DMEM_1_0, PAGE 1
.rofardata > PRU_DMEM_1_0, PAGE 1
.farbss > PRU_DMEM_1_0, PAGE 1
.fardata > PRU_DMEM_1_0, PAGE 1
.resource_table > PRU_DMEM_1_0, PAGE 1
.ShareMemory > PRU_SHAREDMEM, PAGE 2
}
同时在主函数中添加:
#pragma DATA_SECTION(ShareMemRPMsg, "ShareMemory")
RPMsg_protocol_t ShareMemRPMsg;
但编译发现编译器一直寻找不到“ShareMemory”段,请问是我使用的方法有问题吗?
以下是报错信息:
Description Resource Path Location Type
#10247-D creating output section "ShareMemory" without a SECTIONS specification PRU_1_ICSS1_RPMsg C/C++ Problem