你好,目前我们基于TDA3MV设计一款板,用于雷达波的DAC应用,在调试中发现这么一个问题,关于QSPI的配置,我们配置成QSPI_1模式(SYSBOOT15-0:1000000100011000)能量到QPSI_CLK有12M的时钟输出,QSPI_CS也有波形输出,然后能正常烧录SBL文件并正常运行。但是我们切换到QSP_4(SYSBOOT15-0:1000000100011001)模式量QPSI_CLK和QSPI_CS均无波形,正常QPSI_CLK应该有个48M时钟输出。然后烧录的话,能烧录。但是QPSI_4模式烧录时会在verify时会报错,然后运行的话,无法运行,QSPI_CLK一直无波形,然后切换到QSPI_1时,用QSPI_4模式烧录的文件能运行,这个说明当时烧录其实是成功了,只是QSP_4无反应而已。麻烦帮忙ckeck下是哪里的问题。