This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 2g配置

我照默认的文档 DM81xx_DVRRDK_MemoryMap.pdf配置config_2G.bld了,但是在load.sh 时不通过。

 [m3video]  8082: SYSTEM  : FREE SPACE : System Heap      = 6280232 B, Mbx = 0 msgs)
 [m3video]  8082: SYSTEM  : FREE SPACE : SR0 Heap         = 131957632 B (125 MB)
 [m3video]  8083: SYSTEM  : FREE SPACE : Frame Buffer     = 395313024 B (376 MB)
 [m3video]  8083: SYSTEM  : FREE SPACE : Bitstream Buffer = 134217600 B (127 MB)
 [m3video]  8083: SYSTEM  : FREE SPACE : Tiler Buffer     = 0 B (0 MB)  - TILER OFF
 [m3vpss ]  8131: SYSTEM  : FVID2 Init in progress DONE !!!
 [m3vpss ]  8131: SYSTEM  : Device Init in progress !!!
 [m3video]  8107: SYSTEM  : Initializing Links ... DONE !!!
 [m3vpss ] initPrms.isI2cInitReq = 0
 [m3vpss ] initPrms.isI2cInitReq = 0
 [m3vpss ]  8134: SYSTEM  : Device Init in progress DONE !!!
 [m3vpss ]  8255: SYSTEM  : System VPSS Init Done !!!
 [m3vpss ]  8255: UTILS: DMA: HWI Create for INT62 !!!
 [m3vpss ]  8255: SYSTEM  : Initializing Links !!!
 [m3vpss ]  8255: SYSTEM  : FREE SPACE : System Heap      = 13056 B, Mbx = -2 msgs)
 [m3vpss ]  8255: SYSTEM  : FREE SPACE : SR0 Heap         = 131957632 B (125 MB)
 [m3vpss ]  8256: SYSTEM  : FREE SPACE : Frame Buffer     = 391003008 B (372 MB)
 [m3vpss ]  8256: SYSTEM  : FREE SPACE : Bitstream Buffer = 134217600 B (127 MB)

 

配置文件主体为:

/* first 512MB */
LINUX_SIZE                 = 464*MB;
VIDEO_M3_CODE_SIZE         = 2.5*MB;
VIDEO_M3_DATA_SIZE         = 9.5*MB;
DSS_M3_CODE_SIZE           = 2*MB;
DSS_M3_DATA_SIZE           = 15.5*MB;
DSP_CODE_SIZE              = 1.5*MB;
DSP_DATA_SIZE              = 17*MB;


/* second 512MB */
TILER_SIZE                 = 256*MB; /* (128+128) - MUST be aligned on 128MB boundary */ //
SR0_SIZE                   = 128*MB;
SR2_FRAME_BUFFER_SIZE      = 377*MB;
HDVPSS_DESC_SIZE           = 2*MB;
HDVPSS_SHARED_SIZE         = 2*MB;
NOTIFY_SHARED_SIZE         = 2*MB;
REMOTE_DEBUG_SIZE          = 1*MB;


/* third and fourth 512 MB */
SR1_SIZE                   = 128*MB;
SR3_INTRADUCATI_IPC_SIZE   = 128*MB;
LINUX_SIZE_SEGMENT2        = 512*MB;

请问怎么回事,为什么Tiler Buffer     = 0 B (0 MB)  - TILER OFF , 一遇到这个就不过。

  • 你好,

    下面的信息可以在里面找到DM81xx_DVR_RDK_Install_Guide.pdf,请问你是否做了相应的修改?

    816X Platforms: Build configuration for 2GB DDR
    • Open and edit <DVR_RDK_BASE>/dvr_rdk/Rules.make
    • Modify DDR_MEM to DDR_MEM_2048M in place of DDR_MEM_1024M at ifeq ($(PLATFORM),
    ti816x-evm)
    • LINUX_MEM parameter in Rules.make is ignored when DDR_MEM_2048M is selected for DDR_MEM
    • Linux memory in this configuration is to be set in different pools of 128M + 472M. The second pool can be
    increased further based on the virtual memory allocation requirement.
    • This 2GB memory configuration is supported for DVR_RDK_BOARD_TYPE = DM816X_UD_DVR and can be
    verified only on DVR Hardware Ver 0.4 or abov