This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDRAM 数据写入有误 HY57V283220T DM642

大家好,我现在调试自己设计的DM642板子时发现,SDRAM的低八位读写有误,其他位正常,我的原理图应该是没有问题的,因为历届师兄也是这么设计的,而且成功了,我程序也没有问题。经过初步检查,我感觉是DQM位的选通有误,低八位的选通位即DQM0的信号输出不是正常的选择信号,比较杂乱。小弟,也不知道到底哪儿出了问题,有时候选通位正常,能够工作,但是大多数时间是不行的,不知道是不是DM642的BGA虚焊所致,我上网查过,有人也提到过这点,亦或是是否为电源问题,我的电源有点小纹波,烦劳各位大神,帮小弟看看啊~  求~~

  • #1. 你是如何判断是写有问题,而不是读有问题的?或者都有问题?

    #2. 你指的不正常的依据是什么?与DQM1的比较有什么区别?

    #3. 修改匹配电阻,检查焊接情况。

    #4. 电阻纹波范围要求为+-5%。